This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5746: The changes in the AM5746 datasheet

Guru 10095 points
Part Number: AM5746

Tool/software:

Hi Support Team,

I would like to confirm the changes to the AM5746 datasheet.

The following contents have been changed. What is the impact or disadvantage to users compared to before the change?
In particular, the change in 1. seems to be intended to say that defects after mass production are not guaranteed; was the same definition included in the datasheet before the change?

1. Addition of the following note.


(2) Material type: When designated, preproduction parts are prototypes/experimental devices, and are not yet approved or released for full production .
Testing and final process, including without limitation quality assurance, reliability performance testing, and/or process qualification, may not yet be complete, and this item is not a material type. Testing and final process, including without limitation quality assurance, reliability performance testing, and/or process qualification, may not yet be complete, and this item is subject to further changes or possible discontinuation. If available for ordering, purchases will be subject to an additional waiver at checkout, and are intended for early internal evaluation purposes only.
These items are sold without warranties of any kind.

2. “Eco system”; Green has been removed; RoHS only.

Best regards,
Kanae

  • Hello Kanae,

    Your thread has been reassigned. Please expect some delay in response.

    -Josue

  • Hi Kane,

    Can you summarize how you have identified these changes?  Maybe you have an "alert" email from TI?  If yes ...can you send that to me (you can attach as a file)?  Unfortunately I'm not subscribed on that folder so may not be seeing what you're seeing.

    Thanks,
    Kyle

  • Hi Kyle,

    Yes, I checked with myTI Product Alerts <donotreply_myti_product_alerts@ti.com> from TI.
    The email is in Japanese, so the English translation is below.


    Hello KANAE KAWAKAMI ,
    The following information was updated during the week of 2025 16 05
    ---------------------------------------------------------------------------------------------
    Product model number: AM5746

    ----------------------------------------------------------------------------------------------
    - The changes to the data sheet “AM574x SitaraTm Processors Silicon Revision 1.0 Data Sheet (Rev. H)” are as follows:

    1. changes to the Appendix:
    - Appendix: Package Options” has been updated.
    - Appendix: Package Material Information” has been updated.

    Best Regards,
    Kanae

  • Hi Kyle,

    Could you please let me know when you reply?
    I need to report it to may customer.

    Best Regards,
    Kanae

  • Hi Kanae-san,

    There is no actual change in the package.  These are changes only in the documentation and don't have an advantage or disadvantage to the customer.

    Regards,
    Kyle

  • Hi Kyle,

    Thank you for your support!

    I will share it with my customer.

    Best Regards,
    Kanae