Hi all,
I met a problem when I test video decode and display performance in RDK 01.08.00.15.
I run the RDK 01.08.00.15 demo code on TI 816X-EVM, and choose "5: VDEC + VDIS - SD/HD Decode ONLY", then input .ini file to read and decode bitstream files.
The problem is, the display stop update and the FPS for all CH are 0 when I decode some bitstream files for 1CH, 4CH or 8CH (all CH decoded the same file). But the same bitstream file is no problem if I decode for over 16CH.
Can anyone help me to clarify the problem? Thanks.