This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829J: Procedure to change clock source

Part Number: DRA829J


Tool/software:

Dear Ti Team,

We are changing the clock source to many modules through the CLK_SEL field in the corresponding register.
However we would like to clarify if besides setting CLK_SEL bits to change clock source, an additional instruction to trigger RST is also needed.

Can you clarify please, whether we can change parent clock without triggering RST signal to a peripheral afterwards?

Thank you in advance.

Best regards,
António

  • Hi,

    Usually, after stopping the peripheral, you need to change/set the clock.
    We have a Sciclient API call for the module ON/OFF.

    Plese refer to below API Guide of Scliclient for more detials.
    https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/10_01_00_04/exports/docs/pdk_jacinto_10_01_00_25/docs/apiguide/j721e/html/group__SCICLIENT__FMW__PM__IF.html#ga329b967edc51edad7a5ac1a1b86a2035

    Can you clarify please, whether we can change parent clock without triggering RST signal to a peripheral afterwards?

    Parent clock not allowed to change for a few modules, which use the same PLL used by other modules.

    Best Regards,
    Sudheer

  • Hi Sudheer,
    Thanks for your quick response.

    Actually we are not using the API referred in your answer.
    We are performing board configuration on MCU_R5F core only, with no interaction with M3 core (SYSFW).
    This is our sequence:
        1. PLL configuration
        2. Clock selection (it only sets the CLK_SEL bitfield)
        3. Power configuration

    Therefore we have a dedicated interface to select the source clock for each module.
    Using this approach, do we need to trigger a RST signal after changing the parent clock in #2?

    Parent clock not allowed to change for a few modules, which use the same PLL used by other modules.

    Where can we find the list of modules which Parent Clock is not allowed to be changed?
    Are there any modules, that even though they have multiple clock selection options, can't be changed (hardware wise)?

    Thank you.
    António

  • Hi,

    This is our sequence:
        1. PLL configuration
        2. Clock selection (it only sets the CLK_SEL bitfield)
        3. Power configuration

    Are you using "Board_init" with receptive configuration like "BOARD_INIT_PLL", "BOARD_INIT_MODULE_CLOCK"
    The above will use sciclient calls at the end for RM, PM configuration.

    Therefore we have a dedicated interface to select the source clock for each module.
    Using this approach, do we need to trigger a RST signal after changing the parent clock in #2?

    If you are directly changing the clock source of the module, you are supposed to perform a module OFF before the clock change and an ON after.
    Please refer to the TI examples from the SDKs for more details.

    Are there any modules, that even though they have multiple clock selection options, can't be changed (hardware wise)?

    You can change the clock for all modules that have multiple clock sources.

    Parent clock not allowed to change for a few modules, which use the same PLL used by other modules.

    Where can we find the list of modules which Parent Clock is not allowed to be changed?

    What I mean above is that changing of PLL frequency is not allowed, as multiple HSDIVs depend on the PLL frequency.
    When you tried to change the clock frequency, not able to success means that changing of clock is not supported for that.

    Best Regards,
    Sudheer