Part Number: AM3352
Tool/software:
We are planning to replace the AM3352 DDR IC due to its end-of-life (EOL) status. The original DDR is DDR3-1600, and the new one is DDR3-1866. Size is the same. According to the application notes for the AM335x EMIF tools, Steps 1B and 2 indicate that the values depend on the speed bin of the device. Does this mean we need to fill out the excel worksheet again to obtain new parameters? Can't our firmware continue using the existing parameters, given that our system only operates at a bandwidth of 800 Mbps?
Thank you.
Andy