This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62P: DPI RGB24bit Mode LCD support

Part Number: AM62P

Tool/software:

Hi AM62P Champ !

My customer is currently reviewing the interface for connecting RGB-24bit mode on the AM62P.

The following statement only mentions up to RGB18 mode, but I would like a detailed explanation of RGB24bit mode as well.

-------------------------------

7.5.2.1.1.3 Connection

Verify display (RGB) connections.

Interface support includes 12-, 16-, 18-, and 24-bit RGB active matrix displays. When connecting only 16-bit data

to an 18-bit panel (BGR565 to BGR666), connect D0-D4 to B1-B5 on LCD, D5-D10 to G0-G5 on the LCD, and

D11-D15 to R1-R5 on LCD. On the 18-bit panel, connect B0 to B5 and R0 to R5.

-------------------------------

Thanks.

Best Regards, Jack