This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does TI OMX VENC component have interface to set SEI?

Hi,

I am using the DM8168 EVM (EZSDK5.03) to developing video streaming applications based on H.264 encoding. I have some questions:

1. Does TI VENC OMX component provide an interface to set SEI information? It is noted that the TI H.264 encoder does provide such an interface.

2. Is video capturing component (VFCC) providing the time stamp information together with the frame captured?

3. When will the gstreamer for DM8168 be released?

Thanks in advance,
Robert