Tool/software:
Hi TI,
TRM says
"Port mask drop frame is defined to be:
• Any data or MAC control frame
• Any length greater than 32 bytes
• Was dropped by the ALE due to PORT_MASK=0 (was not sent to any destination port)
• The frame could have been dropped due to error or other counted reason, so it could be counted elsewhere"
I have the following questions based on the TRM description above:
- What if the length of frame is less tha 32 bytes, will it be counted in Port mask drop?
- Will Portmask drop also count frames dropped due to CRC error/TX_MEMORY_PROTECT_ERROR?
- What are " other counted reason"?
- Is my understanding correct that "Portmask drop will count total number of frames dropped due to ALE, CRC error, or any other reason at MAC Port (in case of egress from CPSW2G) and Host Port (in case of ingress at CPSW2G)" ?
Looking forward to hearing back from you.
Best regards,
Hasan