Tool/software:
Hi,
I am using SK-AM62 with PSDK 9.2 and would like to confirm the eQEP function of resetting the position counter using the index pin.
I am having trouble with the counter not resetting even after setting IEI.
Here's what I've tried:
# connect GPIO0_41 to EQEP0_A and GPIO0_42 to EQEP0_I # enable GPIO0_41 echo 461 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio461/direction echo 0 > /sys/class/gpio/gpio461/value # enable GPIO0_42 echo 462 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio462/direction echo 0 > /sys/class/gpio/gpio462/value # set UP mode echo increase > /sys/bus/counter/devices/counter0/count0/function # enable position counter echo 1 > /sys/bus/counter/devices/counter0/count0/enable # set IEI 2 (IEI_INITRISING) devmem2 0x23200028 w 0x02088000 # increment counter echo 1 > /sys/class/gpio/gpio461/value echo 0 > /sys/class/gpio/gpio461/value # check current counter cat /sys/bus/counter/devices/counter0/count0/count # trigger Index pin echo 1 > /sys/class/gpio/gpio462/value # check current counter but count is not zero. cat /sys/bus/counter/devices/counter0/count0/count
If you try the same thing with SEI, it works as expected.
# connect GPIO0_41 to EQEP0_A and GPIO0_42 to EQEP0_S # enable GPIO0_41 echo 461 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio461/direction echo 0 > /sys/class/gpio/gpio461/value # enable GPIO0_42 echo 462 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio462/direction echo 0 > /sys/class/gpio/gpio462/value # set UP mode echo increase > /sys/bus/counter/devices/counter0/count0/function # enable position counter echo 1 > /sys/bus/counter/devices/counter0/count0/enable # set SEI 2 (SEI_INITQEPSRISING) devmem2 0x23200028 w 0x08088000 # increment counter echo 1 > /sys/class/gpio/gpio461/value echo 0 > /sys/class/gpio/gpio461/value # check current counter cat /sys/bus/counter/devices/counter0/count0/count # trigger Strobe pin echo 1 > /sys/class/gpio/gpio462/value # check current counter and counter is zero. cat /sys/bus/counter/devices/counter0/count0/count
I would appreciate some advice.
Regards,
Takayuki