This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use ROM Ethernet Boot Mode in TMX320C6678L EVM rev1.0?



Dear Everyone,

Is there any who can teach me how to boot with "ROM EMAC Boot mode"?

I'm have a EVM TMX320C6678L Rev of 1.0.

And I set evm to "ROM Ethernet Boot mode"

All I want to do is to boot this device with .out file already created through this "ROM Ethernet Boot mode"

So I set SW3~6 -> (off, on, off, on)  (on, on, on, off)  (on, on, off, off)  (off, on, on, on) 

I could get BOOTP packet successfully through WireShark.

So, I think I can assign proper IP address to this MAC address.

After that I think I can create a packet with Boot Table Frame Header. But I don't know what is going to be happen if I put data payload with packet

 

Please tell me, Is there any examples which will guide me to boot EVM?.

Please help me to do this