Tool/software:
in the evm board. The SOC set the MIPI line is two line. Right now I need to set the line to 4 line. and i change the line to 4 line.
but I do not know how to set the clock-frequency and link-frequencies. how to set this two data. did there any guide to set this two data. thanks very much
and after set this dts file. the ub953 should be set line number. and did there are some other setting should be config?
clock-frequency = <25000000>;
data-lanes = <1 2 3 4>;
link-frequencies = /bits/ 64 <800000000>;