Tool/software:
Hi,
I’m currently working on getting our custom board to boot. We're using the AM3352, and our design is based on the BeagleBone Black (BBB).
We’ve already addressed the issue of the missing EEPROM with board information by patching the U-Boot SPL, which is now working correctly.
However, we’re now facing another issue: U-Boot hangs at the "DRAM: 512" message and does not proceed further. We're using USB0 to boot the bootloader in order to flash the eMMC on the board. For reference, this process works fine on the BBB.
While we plan to use JTAG for deeper debugging, in the meantime I’ve added some debug logs to the source code. Based on my investigation, the problem appears to occur around this point in the code:
common/board_r.c, in the "init_sequence_r" function array.
#ifdef CONFIG_WINBOND_83C553 initr_w83c553f, #endif initr_barrier, initr_malloc, bootstage_relocate, #ifdef CONFIG_DM initr_dm,
Interestingly, the output seems non-deterministic — in some cases, simply placing a
printf changes the behavior. This leads me to suspect the issue may be timing-related.Here it is the UART0 output:
U-Boot SPL 2014.07-00002-gc3d638d-dirty (May 20 2025 - 10:59:54) Using default environment usb_ether using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in MAC 98:89:24:73:2a:84 HOST MAC de:ad:be:af:00:00 RNDIS ready musb-hdrc: peripheral reset irq lost! high speed config #2: 2 mA, Ethernet Gadget, using RNDIS USB RNDIS network up! BOOTP broadcast 1 BOOTP broadcast 2 Using usb_ether device TFTP from server 192.168.1.9; our IP address is 192.168.1.3 Filename 'uboot'. Load address: 0x807fffc0 Loading: ################################################################# ###################### 449.2 KiB/s done Bytes transferred = 440424 (6b868 hex) U-Boot 2014.07-00002-gc3d638d-dirty (May 20 2025 - 10:59:54) I2C: ready DRAM: 512 MiB
Please let me know if you need more details.
Best regards,
Luís