Part Number: OMAP-L138
Tool/software:
When using NAND Flash boot mode, does the OMAP-L138 ROM bootloader use any form of an Error Correction Code (ECC) mechanism?
Can the OMAP-L138 ROM bootloader enable the ECC feature on the EMIFA?
Can the OMAP-L138 ROM bootloader enable an ECC feature internal to a NAND Flash device?
If this is documented somewhere already, I would be grateful for a link to information.