This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux Kernel Load Address

Other Parts Discussed in Thread: OMAP-L138

Hello!

Can anybody say me proper Linux kernel load address. I have OMAP l138 SOM and try to load Linux. But as I understand u-boot can't run Linux. There is log from u-boot:

U-Boot 2009.11 (Nov 09 2010 - 18:48:43)

I2C:   ready
DRAM:  64 MB
MMC:   davinci: 0
In:    serial
Out:   serial
Err:   serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net:   Ethernet PHY: GENERIC @ 0x00

Hit any key to stop autoboot:  3  2  1  0
8192 KiB M25P64 at 0:0 is now current device
## Booting kernel from Legacy Image at c0700000 ...
   Image Name:   Linux-2.6.33-rc4
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1829020 Bytes =  1.7 MB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...


that's all and Linux didn't start. Also I have AM1820 SOM. For AM1820 Linux starts correctly. Main difference that I have found contains in Load Address and Entry Point. For AM1820 these addresses are C0008000.

What are the correct Load Address and Entry Point for OMAP L138?