Tool/software:
Dear TI team
I am trying to get RPMessage to work on a Yocto-built image for an AM625, but the character device files don't show up in /dev, even though the moudles are loaded and the MCU announced its service. I already had a working example with an image from the company Phytec, but since I am not using their board anymore, I want to go back to a TI-only build. Unfortunately I cannot find any significant difference between the two in order to find the error.
Do you have an idea what I could be missing? Thank you very much!
Please check the text file for information about my system and what I'm doing.
uname -a Linux am62xx-evm 6.1.119-ti-ge4e8b16e66f5 #1 SMP PREEMPT Sat Dec 7 07:14:10 UTC 2024 aarch64 GNU/Linux dmesg | grep rpmsg [ 3.738902] virtio_rpmsg_bus virtio0: rpmsg host is online [ 3.773832] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x1 [ 3.829193] virtio_rpmsg_bus virtio1: rpmsg host is online dmesg | grep remoteproc [ 3.566622] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode [ 3.580849] remoteproc remoteproc0: 5000000.m4fss is available [ 3.709686] remoteproc remoteproc0: powering up 5000000.m4fss [ 3.715889] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 2400160 [ 3.751410] remoteproc remoteproc0: remote processor 5000000.m4fss is now up [ 3.803573] remoteproc remoteproc1: 78000000.r5f is available [ 3.809608] remoteproc remoteproc1: attaching to 78000000.r5f [ 3.843133] remoteproc remoteproc1: remote processor 78000000.r5f is now attached [ 3.947905] remoteproc remoteproc2: 30074000.pru is available [ 3.954315] remoteproc remoteproc3: 30078000.pru is available lsmod | grep rpmsg rpmsg_ctrl 16384 0 - Live 0xffff800001281000 rpmsg_char 16384 1 rpmsg_ctrl, Live 0xffff80000122a000 virtio_rpmsg_bus 20480 0 - Live 0xffff800001171000 rpmsg_ns 16384 1 virtio_rpmsg_bus, Live 0xffff800001119000 cat /sys/class/remoteproc/remoteproc0/name 5000000.m4fss cat /sys/class/remoteproc/remoteproc0/state running ls /sys/class/rpmsg/ rpmsg0 rpmsg_ctrl0 rpmsg_ctrl1 cat /sys/class/rpmsg/rpmsg0/name rpmsg_chrdev ls -l /dev | grep rpmsg <no output, should be rpmsg0, rpmsg1, rpmsg_ctrl0, rpmsg_ctrl1> Searched menuconfig for "rpmsg": # CONFIG_RPMSG_TTY is not set # CONFIG_SND_SOC_FSL_RPMSG is not set # CONFIG_SND_SOC_IMX_RPMSG is not set # CONFIG_CROS_EC_RPMSG is not set # Rpmsg drivers CONFIG_RPMSG=y CONFIG_RPMSG_CHAR=m CONFIG_RPMSG_CTRL=m CONFIG_RPMSG_NS=m CONFIG_RPMSG_MTK_SCP=m CONFIG_RPMSG_QCOM_GLINK=y CONFIG_RPMSG_QCOM_GLINK_RPM=y CONFIG_RPMSG_QCOM_GLINK_SMEM=m CONFIG_RPMSG_QCOM_SMD=y CONFIG_RPMSG_VIRTIO=m CONFIG_RPMSG_PRU=m # end of Rpmsg drivers # Rpmsg virtual device drivers CONFIG_RPMSG_KDRV=y # CONFIG_RPMSG_KDRV_DEMO is not set # CONFIG_RPMSG_KDRV_DISPLAY is not set CONFIG_RPMSG_KDRV_ETH_SWITCH=y # end of Rpmsg virtual device drivers CONFIG_SAMPLE_RPMSG_CLIENT=m Searched menuconfig for "mailbox": CONFIG_ARM_SCMI_TRANSPORT_MAILBOX=y CONFIG_MAILBOX=y CONFIG_APPLE_MAILBOX=y # CONFIG_MAILBOX_TEST is not set Device tree M4F node: m4fss@5000000 { compatible = "ti,am64-m4fss"; reg = <0x00 0x5000000 0x00 0x30000 0x00 0x5040000 0x00 0x10000>; reg-names = "iram\0dram"; ti,sci = <0x05>; ti,sci-dev-id = <0x09>; ti,sci-proc-ids = <0x18 0xff>; resets = <0x07 0x09 0x01>; firmware-name = "am62-mcu-m4f0_0-fw"; wakeup-source; mboxes = <0x08 0x09>; memory-region = <0x0a 0x0b>; phandle = <0x66>; }; Device tree mailbox nodes and more: mailbox@4d000000 { compatible = "ti,am654-secure-proxy"; #mbox-cells = <0x01>; reg-names = "target_data\0rt\0scfg"; reg = <0x00 0x4d000000 0x00 0x80000 0x00 0x4a600000 0x00 0x80000 0x00 0x4a400000 0x00 0x80000>; interrupt-names = "rx_012"; interrupts = <0x00 0x22 0x04>; phandle = <0x12>; }; ... mailbox@43600000 { compatible = "ti,am654-secure-proxy"; #mbox-cells = <0x01>; reg-names = "target_data\0rt\0scfg"; reg = <0x00 0x43600000 0x00 0x10000 0x00 0x44880000 0x00 0x20000 0x00 0x44860000 0x00 0x20000>; status = "disabled"; phandle = <0x76>; }; ... mailbox@29000000 { compatible = "ti,am64-mailbox"; reg = <0x00 0x29000000 0x00 0x200>; interrupts = <0x00 0x4c 0x04 0x00 0x4d 0x04>; #mbox-cells = <0x01>; ti,mbox-num-users = <0x04>; ti,mbox-num-fifos = <0x10>; phandle = <0x08>; mbox-m4-0 { ti,mbox-rx = <0x00 0x00 0x00>; ti,mbox-tx = <0x01 0x00 0x00>; phandle = <0x09>; }; mbox-r5-0 { ti,mbox-rx = <0x02 0x00 0x00>; ti,mbox-tx = <0x03 0x00 0x00>; phandle = <0x0c>; }; }; ... mailbox0_cluster0 = "/bus@f0000/mailbox@29000000"; mbox_m4_0 = "/bus@f0000/mailbox@29000000/mbox-m4-0"; mbox_r5_0 = "/bus@f0000/mailbox@29000000/mbox-r5-0"; Code on the MCU M4F: I am using the following function calls: RPMessage_waitForLinuxReady(SystemP_WAIT_FOREVER); RPMessage_announce(ID_A53_0, localEndpt, "rpmsg_chrdev"); The debugger shows that both functions are called and return with success. The exact same MCU firmware also worked on Phytec's Linux. The SDK version is 09.01.00.39.