Has anyone successfully used the NAND flash on the 814x EVM? I have tried using the CCS NAND flash programmer using the following switch settings:
SW1, SW13: All off. SW2.1 on, SW2.2 off.
With these settings the flash programmer seems to run but it reads 0's for the device id and man. id, and garbage for the other parameters. By enabling SW2.2 I can successfully program the SPI flash using CCS. I have also tried setting SW1 for NAND boot with UART as a fallback mode. In this mode I could successfully load the first stage u-boot via the UART, but the loaded u-boot could not detect a nand part either.
The schematics for the EVM suggests that SW1.7 should be on but I tried that as well without any success. I even tried reseating the flash part in the socket.
If anyone has successfully accessed the flash I would appreciate knowing what your switch settings were. I have a PG2.0 Rev C EVM. Thanks for the help.