Other Parts Discussed in Thread: TVP5150
Hi,
I currently have the following working on a dm365 board:
linux-2.6.32.17-psp03.01.01.38-r47
U-Boot 2009.03-svn1905 (Nov 22 2011 - 12:47:33)
Due to some intermittent nand issues with bootup, we want to upgrade the u-boot to something newer. So I downloaded ti-dvsdk_dm365-evm_4_02_00_06 and tried the prebuilt-images (u-boot-dm365-evm.bin, uImage-dm365-evm.bin) (u-boot-2010.12-rc2-psp03.01.01.39, linux-2.6.32.17-psp03.01.01.39 ) but it fails to boot properly. I got a penguin on the screen but the serial console is all garbage (all 0x00s) after uncompressing the kernel. The interesting thing is that I can get the pre built uImage (linux-2.6.32.17-psp03.01.01.39) to boot proper if I use the old u-boot (U-Boot 2009.03-svn1905).
Any ideas on what's wrong with u-boot-2010.12-rc2-psp03.01.01.39 that would cause the serial output problem and how to fix it??
Thanks!!
Roy
-----------------------------------------------uboot param
baudrate=115200
bootargs=mem=60M console=ttyS0,115200n8 root=/dev/nfs rw nfsroot=192.168.82.1:/home/rlam/nfsroot tvp5150.debug=1 davinci_capture.device_type=4 dm365_imp.oper_mode=0 ip=dhcp
bootcmd=dhcp;bootm
bootdelay=2
bootfile=/tftpboot/uImage
ethact=DaVinci-EMAC
ethaddr=00:40:a6:01:01:82
stderr=serial
stdin=serial
stdout=serial
ver=U-Boot 2010.12-rc2 (Mar 24 2011 - 19:27:17)
----------------------------------------------- serial output
DM36x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000019.
DONE
Jumping to entry point at 0x81080000.
U-Boot 2010.12-rc2 (Mar 24 2011 - 19:27:17)
Cores: ARM 297 MHz
DDR: 243 MHz
I2C: ready
DRAM: 128 MiB
NAND: 512 MiB
MMC: davinci: 0, davinci: 1
Bad block table found at page 131008, version 0x01
Bad block table found at page 262080, version 0x01
Bad block table found at page 130944, version 0x01
Bad block table found at page 262016, version 0x01
nand_read_bbt: Bad block at 0x00000cf60000
nand_read_bbt: Bad block at 0x00000fce0000
nand_read_bbt: Bad block at 0x00001cf60000
nand_read_bbt: Bad block at 0x00001fce0000
Net: Read from EEPROM @ 0x50 failed
Ethernet PHY: GENERIC @ 0x00
DaVinci-EMAC
Hit any key to stop autoboot:0
BOOTP broadcast 1
DHCP client bound to address 192.168.82.57
Using DaVinci-EMAC device
TFTP from server 192.168.82.1; our IP address is 192.168.82.57
Filename '/tftpboot/uImage'.
Load address: 0x80700000
Loading: *#######################################################################################################
############################################
done
Bytes
transferred = 2148124 (20c71c hex)
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Arago/2.6.32.17-psp03.01.01.39/d
Created: 2011-03-25 0:30:27 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2148060 Bytes = 2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ...
OK
Loading Kernel Image ...
OK
OK
Starting kernel ...
Uncompressing Linux........
............................................................
............................................................
............ done, booting the kernel.
\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x00\0x0