This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: Multiple Ethernet port with same MAC Access at U-boot

Part Number: PROCESSOR-SDK-AM335X


Tool/software:

Hi All,

I am facing an issue while accessing etherent I have am335x-icev2 and i deployed two etherent ports (eth0 and eth1).
I am able to ping back at Kernel level from both port.But i cant get same thing at uboot level ,eth0 is working fine at uboot but eth1 is not working when eth0 is connected then eth1 is also working but as linking up at port 0 but independently eth1 is not working .

Please help to solve this issue if possible:

Here is the DTS structure:

&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
slaves = <2>;
active_slave = <1>; //added
// dual_emac; //commented
status = "okay";
};


&davinci_mdio {
pinctrl-names = "default", "sleep";
compatible = "ti,cpsw-mdio","ti,davinci_mdio";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
reset-gpios = <&gpio3 13 GPIO_ACTIVE_HIGH>;
//reset-gpios = <&gpio3 13 GPIO_ACTIVE_HIGH>, <&gpio3 21 GPIO_ACTIVE_HIGH>;
//reset-gpios = <&gpio3 13 GPIO_ACTIVE_LOW>;
reset-delay-us = <2>


};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "rgmii-id";
dual_emac_res_vlan = <1>;
};

&cpsw_emac1 {
phy_id = <&davinci_mdio>, <3>;
phy-mode = "rgmii-id";
dual_emac_res_vlan = <2>;
};
You can see the output when eth0 is connected:

=>ping 192.168.1.20 link up on port 0, speed 100, full duplex Using cpsw device host 192.168.1.20 is alive------->eth1

=> ping 192.168.1.25 link up on port 0, speed 100, full duplex Using cpsw device host 192.168.1.25 is alive------->eth0

when eth0 is not connected:

ping 192.168.1.20 cpsw Waiting for PHY auto negotiation to complete......... TIMEOUT ! mscc_startup ret :-110 before parse status using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in MAC cc:33:31:35:3a:2d HOST MAC de:ad:be:ef:00:00 RNDIS ready ping failed; host 192.168.1.20 is not alive....

 

  • Hi Team

    Please respond to my above query 

    I am getting one phy only even enable active slave 1 it showing only for phy 0

    =>mdio list

    Cpsw:

    0 - Microsemi VSC8531 <--> cpsw

    But I have two phy's

    mii info

    PHY 0x00: OUI = 0x01C1, Model = 0x17, Rev = 0x02, 100baseT, FDX

    PHY 0x03: OUI = 0x01C1, Model = 0x17, Rev = 0x02, 100baseT, FDX

    Please respond asap.