This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Is there any good way to control gpio by name in kernel driver?

Part Number: AM625


Tool/software:

Is there a kernel layer similar to libgpiod that operates GPIO by name?

  • Hi Stephen,

    No, kernel doesn't use GPIO by name.

    In kernel devicetree, gpio pins are specified according to gpio devicetree bindings, for example:

        vdd_sd_dv: regulator-4 {
            ...
            gpios = <&main_gpio0 31 GPIO_ACTIVE_HIGH>;
        };

    Then the kernel driver uses kernel gpiod framework API to initialize and use the GPIO pins.

  • Hi Bin,

    Our project includes many character device drivers using the traditional method (with module_inti and module_exit). I tried to use devm_gpiod_get to access the gpio node defined in the device tree, but it failed to get the gpio.

    Later, I finded that it might be necessary to convert the driver to the platform driver model in order to use the gpiod framework.

    Is this actually the case? Can a driver implemented using the traditional method directly make use of the gpiod framework?

  • Hi Stephen,

    No, you don't have to convert your driver to platform driver to use gpiod API. You can directly use gpiod_* functions implemented in gpio/gpiolib.c, such as gpiod_get(), gpiod_get_optional(), or gpiod_get_index_optional(), etc.

    Search the kernel drivers/ directory for any example.