This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: Create an SD card fron the RTOS

Part Number: SK-TDA4VM


Tool/software:

When using he manual provided trying to build the vision apps for the SK-TDA4VM    9J721EXSKG01EVM
The created sd card won't boot.  

I get this error:  

SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loading Environment from nowhere... OK
Starting ATF on ARM64 core...

NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty
NOTICE: BL31: Built : 04:20:32, Nov 1 2024
I/TC:
I/TC: OP-TEE version: 4.4.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Oct 18 17:45:27 UTC 2024 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: HUK Initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2024.04-ti-ga970f6e51043 (Nov 13 2024 - 14:26:23 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted


U-Boot 2024.04-ti-ga970f6e51043 (Nov 13 2024 - 14:26:23 +0000)

SoC: J721E SR1.1 GP
Model: Texas Instruments J721e EVM
Board: J721EX-EAIK rev B
DRAM: 2 GiB (effective 4 GiB)
Core: 144 devices, 35 uclasses, devicetree: separate
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1
Net: eth0: ethernet@46000000port@1
Hit any key to stop autoboot: 0
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
Card did not respond to voltage select! : -110
mmc_init: -95, time 115
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
Card did not respond to voltage select! : -110
mmc_init: -95, time 72
** Bad device specification mmc 1 **

It seems the RTOS sdk is not able to run on the sk-tda4vm.
  
When building the LINUX  sdk I also had to change the platform=j721e-sk in the common.sh to make the build work.  

Is there a setting in the build_flags.mak or something else that I can change to build and load the rtos on the SK board?  
In the list of valid values for the board I can only see this list but the sk is not available
# PDK board to build for, valid values: j721e_sim j721e_evm j721s2_evm j784s4_evm j742s2_evm am62a_evm j722s_evm
BUILD_PDK_BOARD=$(SOC)_evm