Part Number: AM62L-PROCESSOR-SDK
Other Parts Discussed in Thread: AM62L
Tool/software:
Hi,
I'm trying to download the Linux RT WIC image for AM62L from the SDK download page (tisdk-default-image-am62lxx-evm--rootfs.wic.xz), but the download fails or becomes extremely slow (around 50 KB/s).
I’ve tried multiple browsers (Chrome, Firefox, Edge), on both Windows and Ubuntu. On Windows I've used a download manager software, but it got stuck at 50% twice and was not able to resume. On Ubuntu, I’ve used "wget -c" which resumes the download, but the estimated time is over 2.5 hours and it fails intermittently.
I’ve verified that I have sufficient disk space, and I’ve tested using different stable internet connections, including disabling Windows Defender and firewalls, just in case something was interfering — no improvement. I'm able to download even larger files from other web servers without issues.
The problem seems to affect all SDK downloads from the TI website, not just the AM62L Linux RT SDK. It seems like this could be an issue with the CDN or server delivering the files.
Is there any alternative mirror or method to get this image more reliably?
Thanks in advance