Tool/software:
using the sensor IMX623 output setting is 1920*1536 raw12 30fps.
and add the imx623.c driver into project.
right now check with the MIPI CSI input that the UB960 will output the MIPI signal.
the register share that the signal is already send out from UB960.
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x73 r4
0x06 0x14 0x0b 0x58
but how to modify the app and driver to receive the signal. check with the information here is below:
I need to update the raw and image size in the application. but after power on. the received information below share.
root@am62axx-evm:/opt/edgeai-gst-apps# media-ctl -p
Media controller API version 6.6.58
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 6.6.58
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 7 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:SRGGB8_1X8/1920x1080 field:none]
<- "cdns_csi2rx.30101000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:SRGGB8_1X8/1920x1080 field:none]
-> "30102000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "30102000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "30102000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "30102000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
pad5: Source
-> "30102000.ticsi2rx context 4":0 [ENABLED,IMMUTABLE]
pad6: Source
-> "30102000.ticsi2rx context 5":0 [ENABLED,IMMUTABLE]
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:SRGGB8_1X8/1920x1080 field:none]
<- "imx219 2-003c":0 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:SRGGB8_1X8/1920x1080 field:none]
-> "30102000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
pad3: Source
pad4: Source