Tool/software:
I have successful booted my evm with sd card while It was running I changed the boot pin number Bmode 7 to low and then high suddenly the evm switched off and then when ever I am trying to reboot it with default sd card boot mode its not booting . so I tried uart boot mode I got a string ending with ccc. please guide me how to boot it again using sd card mode.Previously when I was booting from sd card Ld1 was blinking but now Ld1 is not blinking when evm is booting.
If possible, also share with me the steps to boot using eMMC. I am using a Windows system with CCS.