This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM67A: Video Audio Requirements Check

Part Number: AM67A
Other Parts Discussed in Thread: AM67

Tool/software:

Hi AM67A & AM62A Champ !

My customer considers AM62A and AM67A for their next platform of Ground Vehicle, Marine Vehicle, UAS (Unmanned Aire System).

Can you please check the video/audio requirements below?

AM67A AM62A

Image
Processor

Image Compression

H.264 / H.265 (CBR from 64Kbps ~ 80Mbps for H.264/H.265)
MJPEG (MJPEG up to 150Mbps)

Multiple Streaming

Simultanous encoding : 4K(UHD) 30fps + HD 30fps + VGA 30fps + CIF 30fps

Resolutions

Primary stream : 320x240 up to 4K UHD
Secondary stream : 320x240 up to 4K UHD
MJPEG stream : 320x240 up to 4K UHD

Bit Rate

CBR VBR mode

Mirror / Flips

Mirror / Flip / Rotate / D-Zoom / DIS
Crop/custom aspect ratio (Landscape / Portrait mode)

Image Adjustments

WDR / AGC / ACE / Other image adjustment

Still-frame JPEG capture

JPEG Capture (API command or wired trigger)

Evaluate Zone / Spot

Zone / Spot metering modes. Configurable metering location (change which portion of image used for mrtering)

Adjust to full step-change

Adjust to full step-change in optical input within 100mS (Full black to full daylight, etc)

Focus assist mode

focus-peaking to assist in lens focusing

Extra video output

Micro-HDMI or CVBS (NTSC/PAL) output available

Recording mode

Continuous / Pre-alarm & Post-alarm / Schedule record / Motion & trigger

Add-on transceiver board

Consideration for future inclusion of 3G/6G/12G-SDI add-on transceiver board shall be made.

Audio

Input

1ch Input

Compression

PCM (G.711 μ-law) / AAC-LC, up to 44.1KHz @ 96Kbps (configurable)

Text & Graphic
Overlay

Static Text OSD

Camera shall be capable of displaying up to 10 lines of static text, up to 256 characters
per line, in varying size, color, transparency, location.

Dynamic Text OSD

The text can represent GPS and time/date data, recording duration and
other camera-specific data, or dynamic text received over RS-232 or
ethernet according to a predefined command / data format.

Sensor Device

Sony Starvis-2 1/1.8" IMX678-AAQR1 8.40Megapixel, 60fps NIR enhanced Sensor
Sony Starvis 1/2.8" IMX415-AAQR 8.29Megapixel, 60fps
Sony Starvis 1/2.8" IMX515-AAQM 8.46Megapixel, 30-60fps

 

Thanks.

Best Regards, Jack

  • Hi Jack,

    Some issues I see:

    • Depending on the framerate and resolution of the video displayed, neither would be able to display all 3 at the same time.
    • The AM67's VPAC would be unable to handle all of those cameras at once. It could handle 1.
    • The AM62A can't handle above 5MP at 60fps.

    Best,
    Jared