Tool/software:
Hello, I have a few questions regarding the RTC Only Low-Power Mode of AM62L that I would like to ask you.
1.According to the reference manual, in the low-power real-time clock mode only, the power supply of VDDS_RTC and VDD_RTC needs to be maintained. If an independent power supply design is adopted and the customer desires to keep the internal RTC timing function even after the device is powered off, is it sufficient to merely maintain the power supply of VDDS_RTC and VDD_RTC?
2. What is the approximate power consumption in the RTC Only Low-Power mode? Are there any available reference power consumption data?
3. Based on the first point, if only the power supply states of VDDS_RTC and VDD_RTC need to be maintained, can we use a battery pack or a button battery to continuously supply power to VDDS_RTC and VDD_RTC? Will this design affect the subsequent power-on sequence?
Thank you!