This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

If DM3730 can connect the RGB signal IC (for example FPGA through the camera interface) ,How to configure and connect the sch

Other Parts Discussed in Thread: DM3730

If DM3730 can  connect the RGB  signal IC (for example FPGA through the camera interface) ,How to configure and connect the sch?

And I found the DM3730's YUV interface is support 12 Bit ,and if I want to connect the RGB signal FPGA to it ,How can I do ?

Now we want to connect the 24 bit RGB signal FPGA IC to the DM3730 ,if  we can do it ?

And the system is WINCE. If the software and driver must to modify ,and how difficult  is to develope the driver software ?