Part Number: AM623
Tool/software:
Hi,
We're trying to update our U-Boot version. There is a new update "fixup_a53_cpu_freq_by_speed_grade" function which changes A53 clock by checking speed grade of device.
We have "T" grade and "S" grade boards. T grade in 1.25Ghz works fine and boots as expected. With the same firmware the S grade one fails booting. Before this update there was no such function so both devices were booting with the same firmware. I'll put logs below.
What is the problem? Should we change something in ClkTree or RAM configurations to compatible with 1Ghz configuration. Or should we change something in ATF ?
U-Boot SPL 2025.04 (Jan 01 1970 - 01:00:00 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
Changed A53 CPU frequency to 1000000000Hz (S grade) in DT
SPL initial stack usage: 13424 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Starting ATF on ARM64 core...
NOTICE: BL31: v2.1▒▒&+c+
▒+K▒▒L▒▒▒ihѝ BL31: Built : 01:00:00, Jan 1 1970
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Unable to query firmware capabilities (-60)
I/TC:
I/TC: OP-TEE version: 4.2.0 (gcc version 12.2.0 (Debian 12.2.0-14)) #1 Thu Jan 1 01:00:00 UTC 1970 aarch64
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 ti_sci_init:486 Unable to communicate with control firmware (-65523)
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x000f1978 failed
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 tee_otp_get_hw_unique_key:97 Could not get HUK
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x000f19a8 failed
I/TC: Activated SA2UL device
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 sa2ul_init:106 Could not change TRNG firewall owner
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x000f19b0 failed
E/TC:0 0
E/TC:0 0 Core data-abort at address 0x14 (translation fault)
E/TC:0 0 esr 0x96000005 ttbr0 0x9e992000 ttbr1 0x00000000 cidr 0x0
E/TC:0 0 cpu #0 cpsr 0x800003c4
E/TC:0 0 x0 000000009e8f6000 x1 0000000000000000
E/TC:0 0 x2 0000000000000000 x3 0000000000000000
E/TC:0 0 x4 0000000000000050 x5 000000009e982d70
E/TC:0 0 x6 ffffffffffffffb0 x7 000000000007fd20
E/TC:0 0 x8 000000009e982f80 x9 000000009e903000
E/TC:0 0 x10 0000000000000008 x11 000000009e993f30
E/TC:0 0 x12 0000000000000000 x13 000000009e993ec0
E/TC:0 0 x14 0000000000000000 x15 0000000000000000
E/TC:0 0 x16 000000009e81d848 x17 0000000000000000
E/TC:0 0 x18 0000000000000000 x19 000000009e994200
E/TC:0 0 x20 000000009e994208 x21 000000009e8f6000
E/TC:0 0 x22 000000009e8f6000 x23 000000009e8f6ea0
E/TC:0 0 x24 000000009e8f5d60 x25 0000000000000000
E/TC:0 0 x26 0000000000000000 x27 0000000000000000
E/TC:0 0 x28 0000000000000000 x29 000000009e994170
E/TC:0 0 x30 000000009e8180f8 elr 000000009e818108
E/TC:0 0 sp_el0 000000009e994170
E/TC:0 0 TEE load address @ 0x9e800000
E/TC:0 0 Call stack:
E/TC:0 0 0x9e818108
E/TC:0 0 0x9e808aec
E/TC:0 0 0x9e8232d8
E/TC:0 0 0x9e808cb0
E/TC:0 0 Panic 'unhandled pageable abort' at core/arch/arm/kernel/abort.c:582 <abort_handler>
E/TC:0 0 TEE load address @ 0x9e800000
E/TC:0 0 Call stack:
E/TC:0 0 0x9e808f98
E/TC:0 0 0x9e81fcdc
E/TC:0 0 0x9e80787c
E/TC:0 0 0x9e804a5c
Thanks for helping,
Best Regards