Other Parts Discussed in Thread: AM3517
Hello,
i am running u-boot on a am3517. I am facing the problem that after 45 min since power up i have no access to the peripherie which belongs to the L4 interconnect layer.
Everything works (NAND-Flash, Ethernet, I2C, sd-card, ...) until the 45 min are expired. From this point on I can work with U-Boot console via UART and do everythings that runs only in DDR-RAM. As soon I want to access to some peripherie the board stops.
I am running a modified u-boot-port from the am3517evm board.
I found no counter or timer which could be the reason. The time until the board stops is everytime the same.
Has anyone some ideas or had anyone the same problem?
Thank You!