Part Number: AM62P
Other Parts Discussed in Thread: SK-AM62, SYSCONFIG
Tool/software:
Hi,
After reading the MCU+SDK tutorial, I found that the MCU-side program can be compiled, programmed, and debugged using CCS. However, the WKUP-side program is compiled by CCS and is flashed through a flash script. I would like to ask, if I need to use the MCU's UART and the WKUP's UART in a single program, how can I compile, flash, and debug the program? Or is it recommended to place the MCU-side interfaces (UART, I2C, SPI) in one program and the WKUP-side interfaces in another?
BR,
Bomiao