Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM
Tool/software:
Hi,
Today I started to get into SK-TDA4VM development board for edge AI.
Flashed this wic file into microSD card : https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-SK-TDA4VM
When I start the board, it starts without problem, but the thing is even without doing anything it reaches up to 55 degree Celcius.
When I start the custom AI tab for the images, giving a photo to identify it (default photos, like flamingo or elephant), it reaches up to 75 degree Celcius.
The thing is also it cannot identify any image(I tried for 10+ minutes), so that I have to turn off the board.
Is it a normal behaviour? If no what can be the problem of the board?
As you can see from below given photos, all board is on fire.
P.S. I am using 20V 5A type c adapter to supply power to the board.

Thanks for your help in advance,