Tool/software:
Hi.
We´re using AM6422 with UHS-I (up to SDR104) SD-Card on MMCSD1.
We have several peaks in the radiated emission test spectrum which are clearly related to SD-Card, since they where gone when the card was removed.
To reduce those spikes, I want to enable SSC on PLL2.
Are there any restrictions to the max. supported interface performance of the SD-Card when using SSC?
Thank you!
BR,
Christian