Part Number: AM62P
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Please teach me about the configuration of SysConfig:
1. Pull up/Down: Does this field refer to the setting of the internal initializer or the actual design of the hardware?
2. RX: Does this field mean that the pin must be checked when it is input, and if it is output, it will be blank?
3. In the following figure, the 0 in Signals is not checked, and the following pull up/Down and RX fields need to be set to avoid being interfered by EMI.
4. In the figure below, I want to use 3 in Signals as GPIO out, is it good to select Any for Pins settings?