Tool/software:
Is it possible to swap lanes and Pos-Neg for MIPI (CSI2 and DPI) in TDA4VEN?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Is it possible to swap lanes and Pos-Neg for MIPI (CSI2 and DPI) in TDA4VEN?
Hi,
Do you mean on CSIRX or CSITX?
I think CSIRX allows changing lane position, but does not allow polarity change, whereas CSITX allows changing polarity.
Regards,
Brijesh
Thankyou for your reply.
I asked about both CSIRX and DSITX.
Is the following understanding correct?
If DSITX can change polarity, it seems that CSIRX can also do so.
Hi,
No unfortunately, lane swapping is not possible in CSITX. It supports number of output lanes and polarity change for each lane, but lane position cannot be changed.
Regards,
Brijesh
Is the following understanding correct?
If correct, what are the possible variations of Lane swap for RX(CSI)?
hi,
Yes, that's correct. I would suggest to refer to TRM for more information about possible variations.
Regards,
Brijesh
I checked "SPRUJB3A.pdf" and found the following statement.
Isn't the following specification correct?
Hi Furuna-san,
I am really doubtful that CSIRX supports polarity change. and i think this is supported on CSITX, but let me confirm the same.
Regards,
Brijesh
Jadav-san,
Please confirm whether polarity change is possible or not, as it greatly affects circuit design and pattern design.
We look forward to answer from you.
Best regards,
Hi Jadav-san,
What is the status of the confirmation?
We are currently working on the schematic and would appreciate your response by the end of today (6/5 JST).
Best regards,
Hi Furuna-san,
Confirmed with the team the CSIRX can support both the features ie polarity change and lane position change, whereas CSITX supports only polarity change.
My recommendation is to refer to schematics of EVM and make similar connections for CSITX and CSIRX modules.
Regards,
Brijesh
Hi Jadav-san,
Thank you for the confirmation!
I think that polarity change and lane change would be possible through register settings. Could you please provide me with a document that describes the specifications for these settings?
Regards,
Hi Furuna-san,
These registers are available in TRM, but please note it may not be supported in the current CSIRX driver.
Regards,
Brijesh