Part Number: AM5728
Other Parts Discussed in Thread: BEAGLEBOARD-X15
Tool/software:
Hello Team,
I’m working with the AM5728 SoC (BeagleBoard-X15) and currently using the Processor SDK Linux 9.0, which includes kernel 6.x.
My goal is to enable OpenCL offload to the DSP (C66x cores). I have followed the SDK 9 documentation for kernel and root filesystem setup, and I am not able to boot successfully and load DSP firmware via remoteproc.
-
cloclis missing -
libOpenCL.so, headers, and runtime libraries are not present -
No OpenCL examples or documentation appear to be included in the SDK
These components were available in earlier SDK versions (e.g., 6.x,), which supported OpenCL-based DSP offload.
Could you please confirm:
-
Whether OpenCL is still supported for AM5728 in SDK 9?
-
If yes, how can I obtain the OpenCL runtime and tools compatible with SDK 9?
-
If OpenCL has been deprecated, what is the recommended path for heterogeneous compute on the DSP in current SDKs?
Any guidance or updated resources would be greatly appreciated.
Best regards,
Tamilselvan P