Part Number: AM625
Tool/software:
Hi there,
I have a customed board boot fail when i am trying to boot from SD card. All the voltage is correct. Every board are the same. Here is the console output:
U-Boot SPL 2023.04 (Mar 10 2025 - 15:51:09 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
SPL initial stack usage: 13384 bytes
The DDR4 is integrated, so i didn't find any answer in the forum. Can you help to resolve the problem? Thanks!
Michael