Hello,
My device connects two nand flash, which one connects to cs0 the other connects to cs1, and they share other controller pin. When  I use TI CE6 driver (only drive one nand flash) to read block information in the Eboot, sometimes will get wrong information. But it will work correctly, when I take off one nand flash from the device.
If I want to connect two pieces of NAND flash, what needs to  be taken care?