Other Parts Discussed in Thread: CDCM61002
Hello,
The clock generator used in evm816x_Schematics_RevE.pdf (CDCM61002) has LVDS outputs. Can I use HCSL output clock generator and connect it directly to SERDES_CLK pins of C6A8168?
Thank you,
- Robert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CDCM61002
Hello,
The clock generator used in evm816x_Schematics_RevE.pdf (CDCM61002) has LVDS outputs. Can I use HCSL output clock generator and connect it directly to SERDES_CLK pins of C6A8168?
Thank you,
- Robert
I found this in datasheet (document SPRS680A):
When the PCIe interface is used, the SERDES_CLKN/P clock is required to meet the REFCLK AC
specifications outlined in the PCI Express Card Electromechanical Specification (Gen.1 and Gen.2). When
the SATA interface is used, the SERDES_CLKN/P clock is required to meet the specifications in
Table 7-7. When both the PCIe and SATA interfaces are used, both sets of specifications must be met
simultaneously.
An HCSL differential clock source is required to meet the REFCLK AC specifications outlined in the PCI
Express Card Electromechanical Specification, Rev. 2.0, at the input to the AC coupling capacitors. In
addition, LVDS clock sources that are compliant to the above specification, but with the exceptions shown
in Table 7-8, are also acceptable.
I believe this means, yes, I can connect an HCSL clock generator to the SERDES_CLKN/P pins via 100nF series capacitors. Am I right?
Robert,
A high-quality, low-jitter 100-MHz differential clock source is required for the PCIe and SATA PHYs, so as you described above, the key is that it must meet the specifications as described in the SERDES_CLKN/P Input Clock section of the datasheet.
Regards,
Marc