This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: How to configure the MCU-R5 pins SPI Slave using Free-RTOS ?

Part Number: SK-AM62A-LP

Tool/software:

Hi Team,

Kindly provide details steps to configure MCU-R5 pins as SPI Slave using FreeRTOS in MCU-R5 FW.

As per processor datasheet; MCU_MCSPI0 and MCU_MCSPI1 available on Am62Ax processor datasheet for MCU-R5.

Provide working sample example along with it so we can validate the MCU-SPI working or not ?

MCU-SDK-Version:- mcu_plus_sdk_am62ax_09_02_00_38

Note: We are running applications on the MCU-R5 core, along with Linux running on the A-53 core.


Thanks,
Nisarg