What I would like to: Have three HDMI inputs (1080p60 / 148.5 MHz, 2 x 8 bits) connected to the DM8168. Each of the inputs must be routed to the HDVICP2 devices for encoding / compression. Bandwidth reduced outputs from the HDVICP2 devices will have to be streamed over EMAC and/or USB devices.
I guess the best way to do this, is to use the two HDVPSS devices for the video capture from the first two HDMI receivers, but how to I route a third input. ?
Initially I thought that I could use the GPIO ports for this, but as they are limited to 125MHz system clock, I will have to add extra hardware to de-multiplex, and then multiplex internally in the DM8168 before inputting to the third HDVICP2 component. I guess it could be done with DMM tiler 1, but it requires a lot of work.
Is there another easy way to connect a third input ?