Part Number: PROCESSOR-SDK-AM64X
Tool/software:
Hi Team
I have configured TI AM64x board as RC and another TI AM64x board configured as EP. These two boards are connected each other through PCIe interface. TI AM64x RC mode < ----- > TI AM64x EP mode.
I want RC to send interrupt to EP. I gone through the below stuff from TI AM64x reference manual below explanation
Explanation is as below. I want to know where is this VENDOR_SPECIFIC_CONTROL_REG is located . I want to write value to the register.
12.2.2.4.4.3.1 PCIe Core Downstream Interrupts The Vendor Specific Capability signal of the PCIe core, F0_VSEC_INTERRUPT_OUT, is used to generate interrupts to the EP from the RP. The F0_VSEC_INTERRUPT_OUT represents the interrupt for the EP Physical Function 0. This signal is used to generate the PCIE_DOWNSTREAM_PULSE interrupt to the local host. The RP can write to the Vendor Specific Control registers (PCIE_CORE_PFn_I_VENDOR_SPECIFIC_CONTROL_REG) to assert this signal at the EP and this will trigger the PCIE_DOWNSTREAM_PULSE interrupt to the EP host.
Please can some tell me where VENDOR_SPECIFIC_CONTROL_REG is located ?
Regards
Mahantesh