Part Number: M2-CC3351
Other Parts Discussed in Thread: CC3351, SK-AM62-SIP
Tool/software:
Hello All,
I lose the wireless interface wlan0 whenever I patch the kernel for a cc3351.
Main question: Am I patching and building the kernel incorrectly?
We plan to deploy thousands of these Wi-Fi modules starting early next year, so resolving this video streaming issue is critical to our success. We would greatly appreciate your support in addressing this!
Starting info
- Host PC OS: Ubuntu 22.04
- Board: SK-AM62-SIP EVM
- Link: www.ti.com/.../SK-AM62-SIP
- SDK: ti-processor-sdk-linux-am62xxsip-evm-10.01.10.04-Linux-x86-Install.bin
- Under: PROCESSOR-SDK-LINUX-AM62X — Processor SDK Linux for AM62x
- Wifi module: m.2-cc3351
- WiFi patch being used: drivers-cc33xx-update-to-1.0.0.8.patch
Steps I used for Installing SDK, patching, and building kernel + SD img
Summary: install sdk, patch kernel, build a default image, cp the patched kernel and dtbs and replace the non-patched kernel + dbts. Show that wireless interface breaks as a result of cp patched kernel. (NOTE: this happens if I cp any other kernel Image into rootfs/boot
- After installing SDK, we run the following in the root SDK directory.
export ARCH=arm64
export CROSS_COMPILE=$HOME/Desktop/5-7-10x-SDK/linux-devkit/\
sysroots/x86_64-arago-linux/usr/bin/aarch64-oe-linux/aarch64-oe-linux-
- Go into the TI ARM64 kernel tree
cd ~/Desktop/5-7-10x-SDK/board-support/ti-linux-kernel-6.6.58+git-ti
- Start from a clean tree
make mrproper
- Load TI’s baseline + prune fragment
make defconfig ti_arm64_prune.config
- Open menuconfig and save without making changes
make savedefconfig
cp defconfig arch/arm64/configs/defconfig # overwrite generic defconfig
- Create new branch and check it out
- Apply the patch
- Here are the results as well
davidsober@davidsober-AORUS-16X-ASG ~/Desktop/5-30-SDK/board-support/ti-linux-kernel-6.6.58+git-ti [testing-wlan0-showingup*]$ patch -p1 < ~/Downloads/drivers-cc33xx-update-to-1.0.0.8.patch
patching file drivers/bluetooth/Kconfig
patching file drivers/bluetooth/Makefile
patching file drivers/bluetooth/btti_debugfs.c
patching file drivers/bluetooth/btti_drv.h
patching file drivers/bluetooth/btti_main.c
patching file drivers/bluetooth/btti_sdio.c
patching file drivers/bluetooth/btti_sdio.h
patching file drivers/bluetooth/btti_uart.c
patching file drivers/net/wireless/ti/cc33xx/Makefile
patching file drivers/net/wireless/ti/cc33xx/acx.c
patching file drivers/net/wireless/ti/cc33xx/acx.h
patching file drivers/net/wireless/ti/cc33xx/boot.c
patching file drivers/net/wireless/ti/cc33xx/cc33xx_i.h
patching file drivers/net/wireless/ti/cc33xx/cmd.c
patching file drivers/net/wireless/ti/cc33xx/cmd.h
patching file drivers/net/wireless/ti/cc33xx/conf.h
patching file drivers/net/wireless/ti/cc33xx/debugfs.c
patching file drivers/net/wireless/ti/cc33xx/debugfs.h
patching file drivers/net/wireless/ti/cc33xx/io.c
patching file drivers/net/wireless/ti/cc33xx/main.c
patching file drivers/net/wireless/ti/cc33xx/ps.c
patching file drivers/net/wireless/ti/cc33xx/rx.c
patching file drivers/net/wireless/ti/cc33xx/rx.h
- Back to the SDK root and rebuild everything
cd ~/Desktop/5-30-SDK
make clean
make all -j$(nproc)
make linux_stage
- Create the SD card image
sudo bin/create-sdcard.sh
When create-sdcard.sh asks
“ Choose file path to install from
1 ) Install pre-built images from SDK
2 ) Enter in custom boot and rootfs file paths”
We select 1. Install prebuilt image
Then we select “1:tisdk-default-image-am62xxsip-evm.rootfs.tar.xz”
- Modified uEnv.txt in boot partition and pasted this at the bottom
- name_overlays=ti/k3-am625-sk-m2-cc3301.dtbo
- Running ifconfig we can see wlan0 interface shows up
wlan0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether f8:fb:90:13:6c:52 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
- Plug SD card back into host PC then cp our built kernel image and dtb into rootfs/boot
BOOT=/media/$USER/rootfs/boot # ext4 partition already mounted
sudo cp ~/Desktop/5-30-SDK/board-support/built-images/Image $BOOT/
sudo cp -r ~/Desktop/5-30-SDK/board-support/built-images/dtb/ti $BOOT/dtb/
sudo cp /home/davidsober/Desktop/5-30-SDK/board-support/built-images/fitImage \
/media/davidsober/rootfs/boot/fitImage
sync
- Boot and check ifconfig
Result
root@am62xxsip-evm:~# ifconfig
eth0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 08:04:b4:31:13:8a txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
eth1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet 192.168.1.165 netmask 255.255.255.0 broadcast 192.168.1.255
ether 5e:78:4e:13:25:33 txqueuelen 1000 (Ethernet)
RX packets 31 bytes 3314 (3.2 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 13 bytes 2110 (2.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
loop txqueuelen 1000 (Local Loopback)
RX packets 12 bytes 1078 (1.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 12 bytes 1078 (1.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
- Now wireless interface is not appearing anymore
To fully evaluate the WiFi module we need to be able to patch the kernel and keep the wireless interface. This has been the main issue. If you see incorrect steps, please feel free to respond. We are excited to evaluate the cc3351!