Tool/software:
Hi AM623 Champ !
My customer has developed a custom board based on the TI AM6232 SoC. However, the system fails to boot properly — although the kernel starts, it resets during the boot process, resulting in an infinite reboot loop.
Currently, I have not received the schematics or PCB layout for the board. However, I was provided with boot logs from both the EVK (AM6254) and the custom board for comparison. Based on these logs, I can observe that the reset occurs shortly after the kernel begins execution.
The customer mentioned that the following modifications were made:
- The TCA6424ARGJR I/O expander used on the EVK is not populated on the custom board. I2C1-related DTS entries and corresponding PCA953X kernel drivers were removed.
- The EVK uses the AM6254 (quad-core), while the custom board uses AM6232 (dual-core). The DTS was updated to reflect the correct CPU core count.
- Both boot-time and runtime DTS files have been updated.
- Memory configuration is identical to the EVK, so no changes were made.
- No GPIOs affecting the boot process were identified; all relevant ones were modified as needed.
*Custom Board_log.txt
U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13392 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 1856 bytes Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SoC: AM62X SR1.0 HS-FS Model: Texas Instruments AM6232 PNA ### [INFO] Using fixed EEPROM Info: PNA-AM6232, A, 0142 Board: PNA-AM6232 rev A DRAM: 2 GiB Core: 79 devices, 29 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial ### [DEBUG] EEPROM already read, skipping Unidentified board claims PNA-AM6232 in eeprom header Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'uEnv.txt' 20285952 bytes read in 815 ms (23.7 MiB/s) 56491 bytes read in 22 ms (2.4 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK Working FDT set to 8feef000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.6.32-ti-01287-g6de6e418c80e-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Fri Jul 26 14:32:20 UTC 2024 [ 0.000000] KASLR disabled due to lack of seed [ 0.000000] Machine model: Texas Instruments AM6232 PNA [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x00000000f7600000..0x00000000ff5fffff (131072 KiB) map reusable linux,cma [ 0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000 [ 0.000000] OF: reserved mem: 0x000000009c700000..0x000000009c7fffff (1024 KiB) map non-reusable ramoops@9c700000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB [ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009c800000..0x000000009cafffff (3072 KiB) nomap non-reusable ipc-memories@9c800000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009cb00000..0x000000009cbfffff (1024 KiB) nomap non-reusable m4f-dma-memory@9cb00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009cc00000..0x000000009d9fffff (14336 KiB) nomap non-reusable m4f-memory@9cc00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009da00000..0x000000009dafffff (1024 KiB) nomap non-reusable r5f-dma-memory@9da00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-memory@9db00000 [ 0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000 [ 0.000000] OF: reserved mem: 0x00000000ff700000..0x00000000ffffffff (9216 KiB) nomap non-reusable framebuffer@ff700000 [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000008007ffff] [ 0.000000] node 0: [mem 0x0000000080080000-0x000000009c7fffff] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ff6fffff] [ 0.000000] node 0: [mem 0x00000000ff700000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 20 pages/cpu s42920 r8192 d30808 u81920 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 2. [ 0.000000] software IO TLB: mapped [mem 0x00000000f0f00000-0x00000000f4f00000] (64MB) [ 0.000000] Memory: 1772056K/2097152K available (11968K kernel code, 1250K rwdata, 4036K rodata, 2432K init, 502K bss, 194024K reserved, 131072K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.00000 U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13392 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 1856 bytes Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SoC: AM62X SR1.0 HS-FS Model: Texas Instruments AM6232 PNA ### [INFO] Using fixed EEPROM Info: PNA-AM6232, A, 0142 Board: PNA-AM6232 rev A DRAM: 2 GiB Core: 79 devices, 29 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial ### [DEBUG] EEPROM already read, skipping Unidentified board claims PNA-AM6232 in eeprom header Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'uEnv.txt' 20285952 bytes read in 815 ms (23.7 MiB/s) 56491 bytes read in 23 ms (2.3 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK Working FDT set to 8feef000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.6.32-ti-01287-g6de6e418c80e-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Fri Jul 26 14:32:20 UTC 2024 [ 0.000000] KASLR disabled due to lack of seed [ 0.000000] Machine model: Texas Instruments AM6232 PNA [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x00000000f7600000..0x00000000ff5fffff (131072 KiB) map reusable linux,cma [ 0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000 [ 0.000000] OF: reserved mem: 0x000000009c700000..0x000000009c7fffff (1024 KiB) map non-reusable ramoops@9c700000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB [ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009c800000..0x000000009cafffff (3072 KiB) nomap non-reusable ipc-memories@9c800000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009cb00000..0x000000009cbfffff (1024 KiB) nomap non-reusable m4f-dma-memory@9cb00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009cc00000..0x000000009d9fffff (14336 KiB) nomap non-reusable m4f-memory@9cc00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009da00000..0x000000009dafffff (1024 KiB) nomap non-reusable r5f-dma-memory@9da00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-memory@9db00000 [ 0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000 [ 0.000000] OF: reserved mem: 0x00000000ff700000..0x00000000ffffffff (9216 KiB) nomap non-reusable framebuffer@ff700000 [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000008007ffff] [ 0.000000] node 0: [mem 0x0000000080080000-0x000000009c7fffff] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ff6fffff] [ 0.000000] node 0: [mem 0x00000000ff700000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 20 pages/cpu s42920 r8192 d30808 u81920 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 2. [ 0.000000] software IO TLB: mapped [mem 0x00000000f0f00000-0x00000000f4f00000] (64MB) [ 0.000000] Memory: 1772056K/2097152K available (11968K kernel code, 1250K rwdata, 4036K rodata, 2432K init, 502K bss, 194024K reserved, 131072K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80c00000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000080440000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080450000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008616] Console: colour dummy device 80x25 [ 0.013230] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023916] pid_max: default: 32768 minimum: 301 [ 0.028729] LSM: initializing lsm=capability,integrity [ 0.034125] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.041711] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.051926] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1. [ 0.059274] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1. [ 0.067259] rcu: Hierarchical SRCU implementation. [ 0.072169] rcu: Max phase no-delay instances is 1000. [ 0.077840] Platform MSI: msi-controller@1820000 domain created [ 0.084177] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.093601] EFI services will not be available. [ 0.098507] smp: Bringing up secondary CPUs ... [ 0.103911] Detected VIPT I-cache on CPU1 [ 0.104026] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.104044] GICv3: CPU1: using allocated LPI pending table @0x0000000080460000 [ 0.104113] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.104276] smp: Brought up 1 node, 2 CPUs [ 0.133689] SMP: Total of 2 processors activated. [ 0.138505] CPU features: detected: 32-bit EL0 Support [ 0.143783] CPU features: detected: CRC32 instructions [ 0.149113] CPU: All CPU(s) started at EL2 [ 0.153310] alternatives: applying system-wide alternatives [ 0.161322] devtmpfs: initialized [ 0.173461] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.183484] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.195788] pinctrl core: initialized pinctrl subsystem [ 0.202047] DMI not present or invalid. [ 0.207043] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.214173] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.221587] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.229667] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.237888] audit: initializing netlink subsys (disabled) [ 0.243694] audit: type=2000 audit(0.152:1): state=initialized audit_enabled=0 res=1 [ 0.244269] thermal_sys: Registered thermal governor 'step_wise' [ 0.251644] thermal_sys: Registered thermal governor 'power_allocator' [ 0.257842] cpuidle: using governor menu [ 0.268739] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.275747] ASID allocator initialised with 65536 entries [ 0.293181] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@f0000/pinctrl@a40000/cpsw-cpts [ 0.305410] Modules: 27680 pages in range for non-PLT usage [ 0.305432] Modules: 519200 pages in range for PLT usage [ 0.312304] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.324740] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.331150] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.338096] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.344506] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.351445] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.357853] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.364793] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.373034] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected [ 0.382552] iommu: Default domain type: Translated [ 0.387478] iommu: DMA domain TLB invalidation policy: strict mode [ 0.394196] SCSI subsystem initialized [ 0.398517] usbcore: registered new interface driver usbfs [ 0.404169] usbcore: registered new interface driver hub [ 0.409633] usbcore: registered new device driver usb [ 0.415401] pps_core: LinuxPPS API ver. 1 registered [ 0.420488] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.429841] PTP clock support registered [ 0.434033] EDAC MC: Ver: 3.0.0 [ 0.437902] scmi_core: SCMI protocol bus registered [ 0.443301] FPGA manager framework [ 0.446921] Advanced Linux Sound Architecture Driver Initialized. [ 0.454276] vgaarb: loaded [ 0.457557] clocksource: Switched to clocksource arch_sys_counter [ 0.464113] VFS: Disk quotas dquot_6.6.0 [ 0.468165] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.482417] NET: Registered PF_INET protocol family [ 0.487764] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.497054] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.505899] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.513831] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.522062] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear) [ 0.530133] TCP: Hash tables configured (established 16384 bind 16384) [ 0.537094] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.544040] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.551606] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.558100] RPC: Registered named UNIX socket transport module. [ 0.564198] RPC: Registered udp transport module. [ 0.569010] RPC: Registered tcp transport module. [ 0.573823] RPC: Registered tcp-with-tls transport module. [ 0.579432] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.586042] NET: Registered PF_XDP protocol family [ 0.590966] PCI: CLS 0 bytes, default 64 [ 0.596492] Initialise system trusted keyrings [ 0.601399] workingset: timestamp_bits=46 max_order=19 bucket_order=0 [ 0.608441] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.614799] NFS: Registering the id_resolver key type [ 0.620016] Key type id_resolver registered [ 0.624296] Key type id_legacy registered [ 0.628417] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.635279] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.676731] Key type asymmetric registered [ 0.680934] Asymmetric key parser 'x509' registered [ 0.686006] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.693576] io scheduler mq-deadline registered [ 0.698215] io scheduler kyber registered [ 0.702378] io scheduler bfq registered [ 0.709670] pinctrl-single 4084000.pinctrl: 34 pins, size 136 [ 0.716309] pinctrl-single f4000.pinctrl: 171 pins, size 684 [ 0.723843] pinctrl-single a40000.pinctrl: 512 pins, size 2048 [ 0.736688] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled [ 0.754496] loop: module loaded [ 0.759084] megasas: 07.725.01.00-rc1 [ 0.766992] tun: Universal TUN/TAP device driver, 1.6 [ 0.773389] VFIO - User Level meta-driver version: 0.3 [ 0.779883] usbcore: registered new interface driver usb-storage [ 0.786749] i2c_dev: i2c /dev entries driver [ 0.792682] sdhci: Secure Digital Host Controller Interface driver [ 0.799053] sdhci: Copyright(c) Pierre Ossman [ 0.803731] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.810287] ledtrig-cpu: registered to indicate activity on CPUs [ 0.816740] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.824099] usbcore: registered new interface driver usbhid [ 0.829811] usbhid: USB HID core driver [ 0.834158] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100 [ 0.842427] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.851395] optee: probing for conduit method. [ 0.855983] optee: revision 4.2 (12d7c4ee) [ 0.856421] optee: dynamic shared memory is enabled [ 0.866576] random: crng init done [ 0.870187] optee: initialized driver [ 0.876018] NET: Registered PF_PACKET protocol family [ 0.881345] Key type dns_resolver registered [ 0.894480] registered taskstats version 1 [ 0.898871] Loading compiled-in X.509 certificates [ 0.919297] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') [ 0.989700] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz [ 0.996657] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz [ 1.003689] omap_i2c 20020000.i2c: bus 2 rev0.12 at 100 kHz [ 1.009734] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created [ 1.019026] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 1.029074] simple-framebuffer ff700000.framebuffer: framebuffer at 0xff700000, 0x8ca000 bytes [ 1.037932] simple-framebuffer ff700000.framebuffer: format=a8r8g8b8, mode=1920x1200x32, linelength=7680 [ 1.063599] Console: switching to colour frame buffer device 240x75 [ 1.084368] simple-framebuffer ff700000.framebuffer: fb0: simplefb registered! [ 1.093201] ti-udma 485c0100.dma-controller: Number of rings: 82 [ 1.102453] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18) [ 1.114021] ti-udma 485c0000.dma-controller: Number of rings: 150 [ 1.125856] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15) [ 1.136815] printk: console [ttyS2] disabled [ 1.141712] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 239, base_baud = 3000000) is a 8250 [ 1.150754] printk: console [ttyS2] enabled [ 1.150754] printk: console [ttyS2] enabled [ 1.159216] printk: bootconsole [ns16550a0] disabled [ 1.159216] printk: bootconsole [ns16550a0] disabled [ 1.183341] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.229563] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.238735] mdio_bus 8000f00.mdio: MDIO device at address 1 is missing. [ 1.245366] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver unknown [ 1.253260] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006 [ 1.266261] am65-cpsw-nuss 8000000.ethernet: Use random MAC address [ 1.272536] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5 [ 1.279662] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [ 1.286319] pps pps0: new PPS source ptp0 [ 1.290700] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1 [ 1.306437] am65-cps
* Evb_log.txt
U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13392 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 1904 bytes Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SoC: AM62X SR1.0 HS-FS Model: Texas Instruments AM625 SK EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed -121 DRAM: 2 GiB Core: 81 devices, 31 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial EEPROM not available at 0x50, trying to read at 0x51 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 574 bytes read in 20 ms (27.3 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... 20285952 bytes read in 229 ms (84.5 MiB/s) 60191 bytes read in 23 ms (2.5 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK Working FDT set to 8feee000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.6.32-ti-01287-g6de6e418c80e-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Fri Jul 26 14:32:20 UTC 2024 [ 0.000000] KASLR disabled due to lack of seed [ 0.000000] Machine model: Texas Instruments AM625 SK ----------------- EVB kit [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x00000000f7600000..0x00000000ff5fffff (131072 KiB) map reusable linux,cma [ 0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000 [ 0.000000] OF: reserved mem: 0x000000009c700000..0x000000009c7fffff (1024 KiB) map non-reusable ramoops@9c700000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB [ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009c800000..0x000000009cafffff (3072 KiB) nomap non-reusable ipc-memories@9c800000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009cb00000..0x000000009cbfffff (1024 KiB) nomap non-reusable m4f-dma-memory@9cb00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009cc00000..0x000000009d9fffff (14336 KiB) nomap non-reusable m4f-memory@9cc00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009da00000..0x000000009dafffff (1024 KiB) nomap non-reusable r5f-dma-memory@9da00000 [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-memory@9db00000 [ 0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000 [ 0.000000] OF: reserved mem: 0x00000000ff700000..0x00000000ffffffff (9216 KiB) nomap non-reusable framebuffer@ff700000 [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000008007ffff] [ 0.000000] node 0: [mem 0x0000000080080000-0x000000009c7fffff] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ff6fffff] [ 0.000000] node 0: [mem 0x00000000ff700000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 20 pages/cpu s42920 r8192 d30808 u81920 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 4. [ 0.000000] software IO TLB: mapped [mem 0x00000000f0f00000-0x00000000f4f00000] (64MB) [ 0.000000] Memory: 1771864K/2097152K available (11968K kernel code, 1250K rwdata, 4036K rodata, 2432K init, 502K bss, 194216K reserved, 131072K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80c00000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000080440000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080450000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008661] Console: colour dummy device 80x25 [ 0.013282] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023973] pid_max: default: 32768 minimum: 301 [ 0.028804] LSM: initializing lsm=capability,integrity [ 0.034207] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.041799] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.052142] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1. [ 0.059502] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1. [ 0.067481] rcu: Hierarchical SRCU implementation. [ 0.072389] rcu: Max phase no-delay instances is 1000. [ 0.078072] Platform MSI: msi-controller@1820000 domain created [ 0.084471] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.093943] EFI services will not be available. [ 0.098936] smp: Bringing up secondary CPUs ... [ 0.104376] Detected VIPT I-cache on CPU1 [ 0.104487] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.104506] GICv3: CPU1: using allocated LPI pending table @0x0000000080460000 [ 0.104575] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.105467] Detected VIPT I-cache on CPU2 [ 0.105547] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000 [ 0.105561] GICv3: CPU2: using allocated LPI pending table @0x0000000080470000 [ 0.105600] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.106346] Detected VIPT I-cache on CPU3 [ 0.106412] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000 [ 0.106429] GICv3: CPU3: using allocated LPI pending table @0x0000000080480000 [ 0.106465] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.106558] smp: Brought up 1 node, 4 CPUs [ 0.186318] SMP: Total of 4 processors activated. [ 0.191132] CPU features: detected: 32-bit EL0 Support [ 0.196413] CPU features: detected: CRC32 instructions [ 0.201747] CPU: All CPU(s) started at EL2 [ 0.205946] alternatives: applying system-wide alternatives [ 0.214032] devtmpfs: initialized [ 0.227045] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.237082] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.249564] pinctrl core: initialized pinctrl subsystem [ 0.255653] DMI not present or invalid. [ 0.260410] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.267643] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.275041] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.283131] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.291355] audit: initializing netlink subsys (disabled) [ 0.297170] audit: type=2000 audit(0.184:1): state=initialized audit_enabled=0 res=1 [ 0.297762] thermal_sys: Registered thermal governor 'step_wise' [ 0.305104] thermal_sys: Registered thermal governor 'power_allocator' [ 0.311310] cpuidle: using governor menu [ 0.322202] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.329252] ASID allocator initialised with 65536 entries [ 0.347673] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b [ 0.357529] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@f0000/pinctrl@a40000/cpsw-cpts [ 0.368955] platform connector-hdmi: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b [ 0.380521] Modules: 27680 pages in range for non-PLT usage [ 0.380531] Modules: 519200 pages in range for PLT usage [ 0.387256] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.399676] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.406086] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.413026] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.419434] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.426374] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.432782] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.439722] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.447921] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected [ 0.457460] iommu: Default domain type: Translated [ 0.462402] iommu: DMA domain TLB invalidation policy: strict mode [ 0.469092] SCSI subsystem initialized [ 0.473347] usbcore: registered new interface driver usbfs [ 0.479003] usbcore: registered new interface driver hub [ 0.484471] usbcore: registered new device driver usb [ 0.490243] pps_core: LinuxPPS API ver. 1 registered [ 0.495332] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.504687] PTP clock support registered [ 0.508882] EDAC MC: Ver: 3.0.0 [ 0.512743] scmi_core: SCMI protocol bus registered [ 0.518109] FPGA manager framework [ 0.521690] Advanced Linux Sound Architecture Driver Initialized. [ 0.529099] vgaarb: loaded [ 0.532251] clocksource: Switched to clocksource arch_sys_counter [ 0.538823] VFS: Disk quotas dquot_6.6.0 [ 0.542878] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.557181] NET: Registered PF_INET protocol family [ 0.562509] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.571806] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.580646] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.588588] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.596813] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear) [ 0.604956] TCP: Hash tables configured (established 16384 bind 16384) [ 0.611925] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.618862] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.626424] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.632836] RPC: Registered named UNIX socket transport module. [ 0.638929] RPC: Registered udp transport module. [ 0.643742] RPC: Registered tcp transport module. [ 0.648551] RPC: Registered tcp-with-tls transport module. [ 0.654170] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.660764] NET: Registered PF_XDP protocol family [ 0.665683] PCI: CLS 0 bytes, default 64 [ 0.671432] Initialise system trusted keyrings [ 0.676337] workingset: timestamp_bits=46 max_order=19 bucket_order=0 [ 0.683342] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.689668] NFS: Registering the id_resolver key type [ 0.694888] Key type id_resolver registered [ 0.699166] Key type id_legacy registered [ 0.703286] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.710143] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.751551] Key type asymmetric registered [ 0.755752] Asymmetric key parser 'x509' registered [ 0.760823] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.768392] io scheduler mq-deadline registered [ 0.773026] io scheduler kyber registered [ 0.777176] io scheduler bfq registered [ 0.784683] pinctrl-single 4084000.pinctrl: 34 pins, size 136 [ 0.791322] pinctrl-single f4000.pinctrl: 171 pins, size 684 [ 0.798893] pinctrl-single a40000.pinctrl: 512 pins, size 2048 [ 0.811983] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled [ 0.831016] loop: module loaded [ 0.835685] megasas: 07.725.01.00-rc1 [ 0.843831] tun: Universal TUN/TAP device driver, 1.6 [ 0.850198] VFIO - User Level meta-driver version: 0.3 [ 0.856755] usbcore: registered new interface driver usb-storage [ 0.863579] i2c_dev: i2c /dev entries driver [ 0.869869] sdhci: Secure Digital Host Controller Interface driver [ 0.876226] sdhci: Copyright(c) Pierre Ossman [ 0.880953] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.887659] ledtrig-cpu: registered to indicate activity on CPUs [ 0.894165] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.901531] usbcore: registered new interface driver usbhid [ 0.907246] usbhid: USB HID core driver [ 0.911592] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100 [ 0.919968] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.929068] optee: probing for conduit method. [ 0.933666] optee: revision 4.2 (12d7c4ee) [ 0.934046] optee: dynamic shared memory is enabled [ 0.944153] random: crng init done [ 0.947777] optee: initialized driver [ 0.953764] NET: Registered PF_PACKET protocol family [ 0.959092] Key type dns_resolver registered [ 0.972210] registered taskstats version 1 [ 0.976871] Loading compiled-in X.509 certificates [ 0.998307] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') [ 1.054696] ti-sci-clk 44043000.system-controller:clock-controller: recalc-rate failed for dev=81, clk=20, ret=-19 [ 1.086705] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz [ 1.094043] platform connector-hdmi: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b [ 1.104048] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/bridge-hdmi@3b [ 1.113816] i2c 1-003b: Fixed dependency cycle(s) with /connector-hdmi [ 1.120545] i2c 1-003b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000 [ 1.128437] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz [ 1.135813] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz [ 1.141834] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created [ 1.151135] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 1.161276] simple-framebuffer ff700000.framebuffer: framebuffer at 0xff700000, 0x8ca000 bytes [ 1.170121] simple-framebuffer ff700000.framebuffer: format=a8r8g8b8, mode=1920x1200x32, linelength=7680 [ 1.195623] Console: switching to colour frame buffer device 240x75 [ 1.216583] simple-framebuffer ff700000.framebuffer: fb0: simplefb registered! [ 1.225524] ti-udma 485c0100.dma-controller: Number of rings: 82 [ 1.234751] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18) [ 1.246395] ti-udma 485c0000.dma-controller: Number of rings: 150 [ 1.258212] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15) [ 1.269165] printk: console [ttyS2] disabled [ 1.274069] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 239, base_baud = 3000000) is a 8250 [ 1.283086] printk: console [ttyS2] enabled [ 1.283086] printk: console [ttyS2] enabled [ 1.291576] printk: bootconsole [ns16550a0] disabled [ 1.291576] printk: bootconsole [ns16550a0] disabled [ 1.308329] spi-nor spi0.0: s28hs512t (65536 Kbytes) [ 1.313449] 7 fixed-partitions partitions found on MTD device fc40000.spi.0 [ 1.320417] Creating 7 MTD partitions on "fc40000.spi.0": [ 1.325811] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 1.332809] 0x000000080000-0x000000280000 : "ospi.tispl" [ 1.339409] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 1.346101] 0x000000680000-0x0000006c0000 : "ospi.env" [ 1.352499] 0x0000006c0000-0x000000700000 : "ospi.env.backup" [ 1.359492] 0x000000800000-0x000003fc0000 : "ospi.rootfs" [ 1.366281] 0x000003fc0000-0x000004000000 : "ospi.phypattern" [ 1.380007] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.424262] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.436574] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867 [ 1.444688] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867 [ 1.452823] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006 [ 1.465824] am65-cpsw-nuss 8000000.ethernet: Use random MAC address [ 1.472110] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5 [ 1.479238] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [ 1.485885] pps pps0: new PPS source ptp0 [ 1.490260] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1 [ 1.506108] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19 [ 1.517515] platform 31000000.usb: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector [ 1.530864] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 1.536474] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 1.544379] xhci-hcd xhci-hcd.0.auto: USB3 root hub has no ports [ 1.550387] xhci-hcd xhci-hcd.0.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000008000000010 [ 1.559849] xhci-hcd xhci-hcd.0.auto: irq 254, io mem 0x31100000 [ 1.566846] hub 1-0:1.0: USB hub found [ 1.570658] hub 1-0:1.0: 1 port detected [ 1.576792] cpufreq: cpufreq_online: CPU0: Running at unlisted initial frequency: 1200000 KHz, changing to: 1250000 KHz [ 1.590113] mmc0: CQHCI version 5.10 [ 1.597240] pca953x 1-0022: supply vcc not found, using dummy regulator [ 1.604110] pca953x 1-0022: using AI [ 1.632832] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [ 1.636824] debugfs: Directory 'pd:186' with parent 'pm_genpd' already present! [ 1.637153] mmc1: CQHCI version 5.10 [ 1.652230] clk: Disabling unused clocks [ 1.659454] ti-sci-clk 44043000.system-controller:clock-controller: is_prepared failed for dev=81, clk=20, ret=-19 [ 1.672295] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit [ 1.674949] ALSA device list: [ 1.682865] No soundcards found. [ 1.687049] Waiting for root device PARTUUID=076c4a2a-02... [ 1.719246] mmc0: Command Queue Engine enabled [ 1.723736] mmc0: new HS200 MMC card at address 0001 [ 1.729603] mmcblk0: mmc0:0001 S0J56X 14.8 GiB [ 1.735870] mmcblk0: p1 p2 [ 1.739534] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB [ 1.739921] mmc1: new ultra high speed SDR104 SDHC card at address aaaa [ 1.745710] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB [ 1.751839] mmcblk1: mmc1:aaaa SB16G 14.8 GiB [ 1.757095] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (239:0) [ 1.765511] mmcblk1: p1 p2 [ 1.828318] usb 1-1: new low-speed USB device number 2 using xhci-hcd [ 1.963186] EXT4-fs (mmcblk1p2): mounted filesystem df72f9af-f988-4c2d-8305-54ee2c15d38e r/w with ordered data mode. Quota mode: none. [ 1.975591] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 1.984537] devtmpfs: mounted [ 1.989388] Freeing unused kernel memory: 2432K [ 1.994048] Run /sbin/init as init process [ 2.002416] input: PixArt USB Optical Mouse as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.0.auto/usb1/1-1/1-1:1.0/0003:093A:2510.0001/input/input0 [ 2.017945] hid-generic 0003:093A:2510.0001: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-xhci-hcd.0.auto-1/input0 [ 2.225123] systemd[1]: System time before build time, advancing clock. [ 2.269339] NET: Registered PF_INET6 protocol family [ 2.275664] Segment Routing with IPv6 [ 2.279434] In-situ OAM (IOAM) with IPv6 [ 2.318808] systemd[1]: systemd 255.4^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified) [ 2.350715] systemd[1]: Detected architecture arm64. Welcome to Arago 2023.10! [ 2.376787] systemd[1]: Hostname set to <am62xx-evm>. [ 2.387476] systemd[1]: Initializing machine ID from random generator. [ 2.670970] systemd[1]: Configuration file /usr/lib/systemd/system/ti-apps-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.709323] systemd[1]: Configuration file /usr/lib/systemd/system/seva-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.795016] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. [ 2.913843] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. [ 3.000945] systemd[1]: Queued start job for default target Graphical Interface. [ 3.043256] systemd[1]: Created slice Slice /system/getty. [ OK ] Created slice Slice /system/getty. [ 3.067330] systemd[1]: Created slice Slice /system/modprobe. [ OK ] Created slice Slice /system/modprobe. [ 3.091235] systemd[1]: Created slice Slice /system/serial-getty. [ OK ] Created slice Slice /system/serial-getty. [ 3.114420] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 3.136841] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ 3.160704] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ 3.184515] systemd[1]: Expecting device /dev/ttyS2... Expecting device /dev/ttyS2... [ 3.204541] systemd[1]: Reached target Path Units. [ OK ] Reached target Path Units. [ 3.220420] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 3.240429] systemd[1]: Reached target Slice Units. [ OK ] Reached target Slice Units. [ 3.256416] systemd[1]: Reached target Swaps. [ OK ] Reached target Swaps. [ 3.317630] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 3.344693] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 3.374276] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 3.397094] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 3.421909] systemd[1]: Listening on Journal Audit Socket. [ OK ] Listening on Journal Audit Socket. [ 3.445380] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 3.469318] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 3.485563] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 3.513551] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 3.537267] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 3.561293] systemd[1]: Listening on User Database Manager Socket. [ OK ] Listening on User Database Manager Socket. [ 3.616948] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 3.637957] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 3.666539] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 3.685358] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing). [ 3.707547] systemd[1]: Mounting Temporary Directory /tmp... Mounting Temporary Directory /tmp... [ 3.732656] systemd[1]: Starting Create List of Static Device Nodes... Starting Create List of Static Device Nodes... [ 3.763101] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs... [ 3.787312] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm... [ 3.810981] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 3.837043] systemd[1]: Starting Start psplash boot splash screen... Starting Start psplash boot splash screen... [ 3.861363] fuse: init (API version 7.39) [ 3.889279] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 3.909191] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/). [ 3.922297] systemd[1]: Starting Journal Service... Starting Journal Service... [ 3.951903] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 3.985311] systemd[1]: Starting Generate network units from Kernel command line... Starting Generate network units from Kernel command line... [ 4.020889] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems cryptodev: loading out-of-tree module taints kernel. [0m... [ 4.042404] cryptodev: driver 1.13 loaded. [ 4.064204] systemd-journald[122]: Collecting audit messages is enabled. [ 4.079969] systemd[1]: Starting Coldplug All udev Devices... Starting Coldplug All udev Devices... [ 4.108408] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 4.126245] systemd[1]: Started Start psplash boot splash screen. [ OK ] Started Start psplash boot splash screen. [ 4.148948] EXT4-fs (mmcblk1p2): re-mounted df72f9af-f988-4c2d-8305-54ee2c15d38e r/w. Quota mode: none. [ 4.151933] systemd[1]: Mounted Huge Pages File System. [ OK ] Mounted Huge Pages File System. [ 4.183404] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory /tmp. [ OK ] Finished Create List of Static Device Nodes. [ OK ] Finished Load Kernel Module configfs. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [ OK ] Finished Load Kernel Modules. [ OK ] Finished Generate network units from Kernel command line. [ OK ] Finished Remount Root and Kernel File Systems. Mounting FUSE Control File System... Mounting Kernel Configuration File System... [ OK ] Started Start psplash-systemd progress communication helper. Starting Flush Journal to Persistent Storage... Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev gr[ 4.626298] systemd-journald[122]: Received client request to flush runtime journal. acefully... [ OK ] Mounted FUSE Control File System. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Finished Apply Kernel Variables. [ OK ] Finished Create Static Device Nodes in /dev gracefully. Starting Create System Users... [ OK ] Finished Coldplug All udev Devices. [ 4.899960] audit: type=1334 audit(1709054766.668:2): prog-id=6 op=LOAD [ 4.906697] audit: type=1334 audit(1709054766.676:3): prog-id=7 op=LOAD [ 4.913378] audit: type=1334 audit(1709054766.684:4): prog-id=8 op=LOAD Starting User Database Manager... [ OK ] Started User Database Manager. [ OK ] Finished Create System Users. Starting Create Static Device Nodes in /dev... [ OK ] Finished Create Static Device Nodes in /dev. [ OK ] Reached target Preparation for Local File Systems. Mounting /var/volatile... [ 5.251967] audit: type=1334 audit(1709054767.020:5): prog-id=9 op=LOAD [ 5.258735] audit: type=1334 audit(1709054767.028:6): prog-id=10 op=LOAD Starting Rule-based Manager for Device Events and Files... [ OK ] Mounted /var/volatile. Starting Load/Save OS Random Seed... [ OK ] Reached target Local File Systems. Starting Rebuild Dynamic Linker Cache... Starting Create Volatile Files and Directories... [ OK ] Finished Load/Save OS Random Seed. [ OK ] Finished Create Volatile Files and Directories. Starting Rebuild Journal Catalog... [ 5.555010] audit: type=1334 audit(1709054767.324:7): prog-id=11 op=LOAD Starting Network Name Resolution... [ 5.578895] audit: type=1334 audit(1709054767.348:8): prog-id=12 op=LOAD Starting Network Time Synchronization... Starting Record System Boot/Shutdown in UTMP... [ OK ] Started Rule-based Manager for Device Events and Files. [ OK ] Finished Record System Boot/Shutdown in UTMP. [ OK ] Finished Rebuild Journal Catalog. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Set. [ OK ] Started Network Name Resolution. [ OK ] Reached target Host and Network Name Lookups. [ OK ] Found device /dev/ttyS2. [ 7.539095] at24 0-0051: supply vcc not found, using dummy regulator [ 7.569671] at24 0-0051: 65536 byte 24c512 EEPROM, writable, 1 bytes/write [ 7.577497] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.590032] tps6598x 0-003f: Unable to find the interrupt, switching to polling [ 7.608320] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.631733] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.642339] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.652799] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000 [ 7.662842] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode [ 7.671825] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device [ 7.691144] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.701084] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.711181] remoteproc remoteproc0: 5000000.m4fss is available [ 7.713632] rtc-ti-k3 2b1f0000.rtc: registered as rtc0 [ 7.713840] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.713875] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.723935] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.732689] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:13 UTC (13) [ 7.739670] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.740723] remoteproc remoteproc0: powering up 5000000.m4fss [ 7.740754] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 55016 [ 7.746874] systemd-journald[122]: Time jumped backwards, rotating. [ 7.757739] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node m4f-dma-memory@9cb00000 [ 7.794780] virtio_rpmsg_bus virtio0: rpmsg host is online [ 7.795753] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.800509] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [ 7.809204] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.816866] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ 7.832959] rproc-virtio rproc-virtio.2.auto: registered virtio0 (type 7) [ 7.834600] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.840086] remoteproc remoteproc0: remote processor 5000000.m4fss is now up [ 7.848900] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.883689] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.892304] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ OK ] Reached target Hardware activated U[ 7.912786] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ 7.934951] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 7.943876] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 7.953273] platform 78000000.r5f: configured R5F for IPC-only mode [ 7.993171] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000 [ 8.020939] sii902x 1-003b: supply iovcc not found, using dummy regulator [ 8.028407] sii902x 1-003b: supply cvcc12 not found, using dummy regulator [ 8.036956] remoteproc remoteproc1: 78000000.r5f is available [ 8.045133] i2c i2c-1: Added multiplexed i2c bus 3 [ 8.054598] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports [ 8.065576] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports [ 8.076754] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0 [ 8.083483] remoteproc remoteproc1: attaching to 78000000.r5f [ 8.084904] tidss 30200000.dss: [drm] Cannot find any crtc or sizes [ 8.097516] tidss 30200000.dss: [drm] Cannot find any crtc or sizes [ 8.104477] PVR_K: 188: Device: fd00000.gpu [ 8.110920] platform 78000000.r5f: R5F core initialized in IPC-only mode [ 8.118611] rproc-virtio rproc-virtio.4.auto: assigned reserved memory node r5f-dma-memory@9da00000 [ 8.128658] PVR_K: 188: Read BVNC 33.15.11.3 from HW device registers [ 8.136872] PVR_K: 188: RGX Device registered with BVNC 33.15.11.3 [ 8.137491] virtio_rpmsg_bus virtio1: rpmsg host is online [ 8.138477] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd [ 8.138725] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe [ 8.166422] rproc-virtio rproc-virtio.4.auto: registered virtio1 (type 7) [ 8.174886] remoteproc remoteproc1: remote processor 78000000.r5f is now attached [ 8.190374] [drm] Initialized pvr 24.1.6554834 20170530 for fd00000.gpu on minor 1 [ 8.373151] remoteproc remoteproc2: 30074000.pru is available [ 8.382436] remoteproc remoteproc3: 30078000.pru is available Starting Virtual Console Setup... [ OK ] Stopped Virtual Console Setup. Starting Virtual Console Setup... [ OK ] Finished Rebuild Dynamic Linker Cache. Starting Update is Completed... [ OK ] Finished Update is Completed. [ OK ] Finished Virtual Console Setup. [ OK ] Created slice Slice /system/systemd-fsck. Expecting device /dev/mmcblk0p1... [ OK ] Reached target System Initialization. [ OK ] Started Daily rotation of log files. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timer Units. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API... [ OK ] Listening on dropbear.socket. [ OK ] Listening on PC/SC Smart Card Daemon Activation Socket. Starting Weston socket... [ 9.019614] audit: type=1334 audit(14.784:9): prog-id=13 op=LOAD Starting D-Bus System Message Bus... Starting Reboot and dump vmcore via kexec... [ OK ] Listening on Docker Socket for the API. [ OK ] Listening on Weston socket. [ OK ] Finished Reboot and dump vmcore via kexec. [ OK ] Started D-Bus System Message Bus. [ 9.146471] dbus-broker-lau[557]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set [ OK ] Found device /dev/mmcblk0p1. Expecting device /dev/mmcblk1p1... [ OK ] Reached target Socket Units. [ OK ] Reached target Basic System. Starting Save/Restore Sound Card State... [ OK ] Started Job spooling tools. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Periodic Command Scheduler. Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ OK ] Started irqbalance daemon. Starting Telephony service... Starting Expand the rootfs partiti��to full size of the boot device.... [ OK ] Started Seva Launcher Service. [ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf. Starting File System Check on /dev/mmcblk0p1... [ 9.520511] audit: type=1334 audit(15.288:10): prog-id=14 op=LOAD [ 9.532910] audit: type=1334 audit(15.300:11): prog-id=15 op=LOAD [ 9.539223] audit: type=1334 audit(15.304:12): prog-id=16 op=LOAD Starting User Login Management... Starting Telnet Server... [ OK ] Started ti-apps-launcher service. [ OK ] Finished Save/Restore Sound Card State. [ OK ] Finished IPv6 Packet Filtering Framework. [ OK ] Finished IPv4 Packet Filtering Framework. [ OK ] Finished Telnet Server. [ OK ] Found device /dev/mmcblk1p1. [ OK ] Finished File System Check on /dev/mmcblk0p1. [ OK ] Started Telephony service. [ OK ] Reached target Preparation for Network. [ OK ] Reached target Sound Card. Mounting /run/media/mmcblk0p1... Starting PulseAudio Sound System... Starting File System Check on /dev/mmcblk1p1... [ 9.795852] audit: type=1334 audit(15.560:13): prog-id=17 op=LOAD Starting Network Configuration... [ OK ] Mounted /run/media/mmcblk0p1. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [ 9.918471] Bluetooth: Core ver 2.22 [ 9.922301] NET: Registered PF_BLUETOOTH protocol family [ 9.927743] Bluetooth: HCI device and connection manager initialized [ 9.934213] Bluetooth: HCI socket layer initialized [ 9.939159] Bluetooth: L2CAP socket layer initialized [ 9.944808] Bluetooth: SCO socket layer initialized [ OK ] Started User Login Management. [ 10.217894] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 10.245745] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 10.253068] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600' [ OK ] Finished File System Check on /dev/mmcblk1p1. Mounting /run/media/boot-mmcblk1p1... [ OK ] Started Network Configuration. [ OK ] Reached target Network. [ 10.501298] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL) [ 10.510860] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode Starting Enable and configure wl18xx bluetooth stack... [ 10.536756] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL) [ 10.547766] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode [ OK ] Started Netperf Benchmark Server. Starting Simple Network Management Protocol (SNMP) Daemon.... Starting Permit User Sessions... [ OK ] Finished Enable and configure wl18xx bluetooth stack. [ OK ] Finished Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... Starting Weston, a Wayland compositor, as a system service... [ OK ] Mounted /run/media/boot-mmcblk1p1. [ OK ] Finished Synchronize System and HW clocks. [ OK ] Created slice User Slice of UID 1000. Starting User Runtime Directory /run/user/1000... [ OK ] Finished User Runtime Directory /run/user/1000. Starting User Manager for UID 1000... [ OK ] Started PulseAudio Sound System. [ 11.745165] audit: type=1006 audit(17.512:14): pid=684 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1 [ 11.757209] audit: type=1300 audit(17.512:14): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffd64edc58 a2=4 a3=1 items=0 ppid=1 pid=684 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" key=(null) [ 11.783407] audit: type=1327 audit(17.512:14): proctitle="(systemd)" [ 11.894294] EXT4-fs (mmcblk1p2): resizing filesystem from 2896815 to 3856512 blocks [ 12.273931] EXT4-fs (mmcblk1p2): resized filesystem to 3856512 [ OK ] Finished Expand the rootfs partition to full size of the boot device.. [ OK ] Started Simple Network Management Protocol (SNMP) Daemon.. [ OK ] Started User Manager for UID 1000. [ OK ] Started Session c1 of User weston 13.086064] audit: type=1006 audit(18.852:15): pid=671 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1 0m. [ 13.099008] audit: type=1300 audit(18.852:15): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffcf5c8508 a2=4 a3=1 items=0 ppid=1 pid=671 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/usr/lib/systemd/systemd-executor" key=(null) [ 13.125254] audit: type=1327 audit(18.852:15): proctitle="(weston)" [ 13.361262] PVR_K: 671: RGX Firmware image 'rgx.fw.33.15.11.3' loaded [ 13.381422] PVR_K: 671: Shader binary image 'rgx.sh.33.15.11.3' loaded [ OK ] Started containerd container runtime. [ 13.642476] am65-cpsw-nuss 8000000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx [FAILED] Failed to start Weston, a Wayland compositor, as a system service. See 'systemctl status weston.service' for details. Starting Weston, a Wayland compositor, as a system service... [ OK ] Started Session c2 of User weston 13.887490] audit: type=1006 audit(19.652:16): pid=718 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=3 res=1 0m. [ 13.900442] audit: type=1300 audit(19.652:16): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=fffff89dd798 a2=4 a3=1 items=0 ppid=1 pid=718 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=3 comm="(weston)" exe="/usr/lib/systemd/systemd-executor" key=(null) [ 13.926493] audit: type=1327 audit(19.652:16): proctitle="(weston)" [FAILED] Failed to start Weston, a Wayland compositor, as a system service. See 'systemctl status weston.service' for details. Starting Weston, a Wayland compositor, as a system service... [ OK ] Started Session c3 of User weston 14.233360] audit: type=1006 audit(20.000:17): pid=723 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=4 res=1 0m. [FAILED] Failed to start Weston, a Wayland compositor, as a system service. See 'systemctl status weston.service' for details. Starting Weston, a Wayland compositor, as a system service... [ OK ] Started Session c4 of User weston. [FAILED] Failed to start Weston, a Wayland compositor, as a system service. See 'systemctl status weston.service' for details. Starting Weston, a Wayland compositor, as a system service... [ OK ] Started Session c5 of User weston. [FAILED] Failed to start Weston, a Wayland compositor, as a system service. See 'systemctl status weston.service' for details. [FAILED] Failed to start Weston, a Wayland compositor, as a system service. See 'systemctl status weston.service' for details. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPL-3.0 packages: adwaita-icon-theme _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project am62xx-evm ttyS2 Arago 2023.10 am62xx-evm ttyS2 am62xx-evm login: [ 16.937840] kauditd_printk_skb: 8 callbacks suppressed [ 16.937861] audit: type=1701 audit(22.704:20): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=611 comm="ti-apps-launche" exe="/usr/bin/ti-apps-launcher" sig=11 res=1 [ 16.997899] audit: type=1334 audit(22.764:21): prog-id=18 op=LOAD [ 17.004113] audit: type=1334 audit(22.768:22): prog-id=19 op=LOAD [ 17.010320] audit: type=1334 audit(22.776:23): prog-id=20 op=LOAD [ 21.512498] audit: type=1334 audit(27.280:24): prog-id=20 op=UNLOAD [ 21.518860] audit: type=1334 audit(27.280:25): prog-id=19 op=UNLOAD [ 21.525280] audit: type=1334 audit(27.280:26): prog-id=18 op=UNLOAD
Thanks.
Regards,
Jack