This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7-Q1: The AM62A exhibits yellow pixel artifacts when displaying image content.

Part Number: AM62A7-Q1

Tool/software:

Hi,

We attempted to connect a camera using the AM62A chip and display its output. ​​When using GStreamer to render the image content on-screen​​, yellow pixel artifacts appear on the display.

​Through observation​​, we found that:

  • These artifacts occur in ​​regions with abrupt color changes​
  • They typically manifest at ​​color transition boundaries​​ within the image
  • Example scenario: At the ​​junction line​​ between a white wall and a red door

It is clear from the image that numerous yellow pixel artifacts appear on the brown clothing, which ​​should not exist in normal rendering​​.

I have verified the root cause through the following experimental steps:

  1. ​Display assembly replacement​​:
    After swapping both the screen and its flex cable, ​​the issue persists​​, eliminating display hardware as the cause.
  2. ​Camera substitution​​:
    Using alternative camera modules yielded ​​no improvement​​, excluding camera sensor defects.
  3. ​EdgeAI UI validation​​:
    Directly displaying the ​​EdgeAI interface​​ on screen still produced yellow pixel artifacts.
  4. ​Bridge chip test pattern verification​​:
    Outputting test patterns via the ​​LT9211C bridge chip​​ resulted in ​​artifact-free rendering​​.

​Conclusion​​:
Based on this evidence, I suspect the anomaly originates within TI's ​​Display Rendering Module (DRM)​​. Request TI engineering support to investigate potential DRM-related causes.

The software version I am using is ​​SDK 10.1​​, and my ​​image display pipeline​​ is structured as follows:
​Camera → Gstreamer → DRM → LT9211C Bridge Chip → Display Panel​​.

We look forward to your prompt feedback and technical guidance.

Thanks,

Yuwei