Part Number: AM6422
Tool/software:
Hi.
We have some radiated emission peaks which are clearly related to SD-Card (HS mode, 50MHz)
For testing, I want to slightly reduce the SD-Card frequency, so that there is no "peak overlapping" in the radiated spectrum with other interferers.
Is it possible to change the PLL2_HSDIV_clkout2 divider from 10 to 11 to get 180MHz base frequency instead of 200MHz?
The divider factors for the SD-Host controller remain unchanged, so a High-speed card should be clocked with 180MHz/4 = 45MHz, not 50MHz
Is this possible?
Are there better options to slightly reduce the SD-frequency available?
Thank you,
Christian