This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816X kernel booting error



I got the fowllowing error in bold letter always when i boot ..Please help me on this

 

regulator_init_complete: disabling VFB
ata1: SATA link down (SStatus 0 SControl 300)

 

ata2: SATA link down (SStatus 0 SControl 300)
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f013)
IP-Config: Complete:
     device=eth0, addr=10.10.25.7, mask=255.255.254.0, gw=10.10.24.1,
     host=netra_v, domain=, nis-domain=(none),
     bootserver=10.10.25.4, rootserver=10.10.25.4, rootpath=
PHY: 0:01 - Link is Up - 100/Full
VFS: Mounted root (nfs filesystem) on device 0:14.
devtmpfs: error mounting -2
Freeing init memory: 196K
Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace:
[<c0047b58
>] (dump_backtrace+0x0/0x110) from [<c03685a8>] (dump_stack+0x18/0x1c)
 r7:00000013 r6:c006dc4c r5:c0008670 r4:c04df710
[<c0368590>] (dump_stack+0x0/0x1c) from [<c036860c>] (panic+0x60/0x17c)
[<c03685ac>] (panic+0x0/0x17c) from [<c0039574>] (init_post+0xa4/0xc4)
 r3:c4b4c700 r2:00000000 r1:c05af980 r0:c041eb8d
[<c00394d0>] (init_post+0x0/0xc4) from [<c0008788>] (kernel_init+0x118/0x154)
 r5:c0008670 r4:c04def80
[<c0008670>] (kernel_init+0x0/0x154) from [<c006dc4c>] (do_exit+0x0/0x5e4)
 r5:c0008670 r4:00000000