This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5535 DSP



My ISR on INT0 and INT1 triggers on falling edge.

Is there any register to change this to rising edge

  • Hi

    Would somebody from TI please reply to this post

    Thanks

  • Hi Microt,

    Sorry for the delay.

    The interrupt signals on the external interrupts pins (INT0 and INT1) are detected with a synchronous negative edge detector circuit. To reliably detect the external interrupts, the interrupt signal must have at least 2 SYSCLK high followed by at least 2 SYSCLK low.

    INT0 and INT1 require external pull-ups.

    So I do not think you can interrupt on a rising edge.

    GPIO interrupts are falling or rising edge triggered interrupts.

    I will confirm with the design team.

    Regards,
    Mark

  • Hi Microt,

    I have confirmed that INT0/1 must be on falling edge as documentation dictates. Sorry.

    Some glue logic (mosfet) can invert the polarity of your INT source. Or GPIO interrupt if it works for you.

    Best Regards,
    Mark