Other Parts Discussed in Thread: DRA821
Tool/software:
SERDES_REFCLK has internal termination 40 - 62.5ohm, how can I disable it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
SERDES_REFCLK has internal termination 40 - 62.5ohm, how can I disable it?
Hi Max,
You should be able to disable the ref clk using the SERDES_RST register bit 27: REFCLK_TERM_DIS.
You could refer to the TRM of the J721s2 in the section of SERDES_10G below: The offset and the base address will need to be adjusted based on the DRA821 setting.
https://www.ti.com/product/TDA4VE-Q1
I looked into the DRA821 datasheet and the SERDES registers are still to be populated. I will reach out internally to get this populated.