This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MT29F16G08CBACA id

hi all

hi i  am new to dm365.with dm365 i am using a MT29F16G08CBACA nand device.but when i am flashing into that i am getting error target write verify failed.So can tell me how to define in the nand_ids.c and how to solve the problem

  • HI chakravarthy,

    I 'm also using the same nand flash, which you have posted!!!!!!!!!!!!

    I'm also trying to get the device id through the u-boot source code!!!!!!!!

    Not succeeded!!!!!

    Can you got the solution for this?

    Regards,

    santosh vastrad

  • Hi All,

    I am also facing very similar issue which Chakravarti has mentioned. I have a board which is customized version of DM355 EVM board having MT29F16G08CBACA NAND flash. When I try to flash UBL and u-Boot using "sfh_DM35x.exe" utility, it gives me an error indicating that "Write verify failed. Skipping block!!"

    I have looked in to the reference manual of DM355 EVM and it is mentioned that its RBL (Rom boot-loader) does not support NAND having page size more than 2K (But the flash I am using -MT29F16G08CBACA is of 4K page size). So my queries are:

    1. Have RBL been upgraded to support NAND flash with 4K page size? If Yes then from where can I download this upgraded RBL and how to flash it on board?
    2. What are the other alternatives to support the flash with 4K page size ? Do I need to make any changes in UBL/u-Boot code? If Yes, can you please address me a proper reference document for such changes?
    Thanks,
    Rajesh