This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H264: encode big resolution



Hello!

I have to encode big resolution, from 1Mpx (1280x1024) to 5 Mpx(2560x2048), in H264 and view video via RTSP, I have use live555 and Appro software. I succsefully get 3 Mpx (2048x1536), but with 4 Mpx (2368x1744) and 5 Mpx (2560x2048) I have small problem - I havn't error  when I encode data, but I see only vertical lines.

Where can I found recomendation or sample code for encode 4 Mpx (2368x1744) and bigest resolution?

Thank you and excuse me for my bad english.

  • You must use latest Encode Library of H.264, V2.20. It support 4096x4096 resolution H.264 encode.

  • Thank you for your reply!

    I use latest H264 codec and I have problem with image, but not with encode.

    And I solve this problem:
    h264_encoder_dm365_userguide.pdf (p. 80, 4-32):
    Note:
    In case of encodingPreset = XDM_HIGH_QUALITY, encoder supports
    encoding upto 4096x4096 resolution (MegaPixel). To enable Mega Pixel
    encoding, maxWidth should be given more than 2048 pixels. If
    Megapixel encoding is enabled SVC-T is disable internally.
    In case of encodingPreset =0 or encodingPreset =
    XDM_HIGH_SPPED, encoder support encoding upto 2048x2048
    resolution.