Dear sirs,
My company is developing a camera on 8148 platform. The video front is a CCD that output via two channels. Each output channel is 12bit parallel interface and format is RAW BAYER.
The DM8148 have one camera interface and two VIP. In Chapter 11 of TMS320DM814x DaVinci Digital Media Processors Technical Reference Manual, it describes that the VIP only capture YUV and RGB format data. Can it capture 12bit raw data ? How to do it?
If yes, I want to use the two VIP to capture raw data from the two channels, save raw data to DDR and then merge the two channels raw data into one complete raw data, and process the complete raw data with ISS.
If no, can you advice us a solution of two channels raw data on 8148?
Kind regards,
Yang Jun
Shenzhen Intelligent Imaging Electronics Co.,Ltd