Hi,
We are interested in migrate our c6727 codes to a c6745 DSPs. We use mainly floating point routines (adaptative filters, eco cancellers, clock recovery system, and so on).
We've seen in the data sheet that 6747 is compatible with c67x+ set of instructions and also that it has a large MFLOPS figure.
We'd like to know if the 6745 will be capable of improving our C6727 performance which is almost full in processing time between real time interrupts (90%) and IRAM (95%).
We guess that it will be even better (faster and more IRAM) but due to this fixed point compatibility we are wondering if this can cause a poorer floating performance compared to a pure floating processor such as c6727.
Any experience comparing this DSPs in intensive floating point processing???
Thanks a lot